This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

wl1271L TiWi-BLE WLAN driver for dm3730

Other Parts Discussed in Thread: DM3730, OMAP3530, WL1271

Hi,

I have designed a DM3730 based board taking reference from the Mistral omap3evm board. I have connected WLAN module (WL1271L TiWi-BLE module from LS Research) connected to the MMC2 port. I have mapped the WLAN_IRQ pin at MMC2_DAT5/GPIO_137 pin(used as GPIO) and the WLAN_EN pin at MMC2_DAT7/GPIO_139 pin(used as GPIO). I have made corresponding changes in the file "arch/arm/mach-omap2/board_omap3evm.c".

I am having problem driving the WLAN module using Linux Kernel 2.6.37 available in DM3730 DVSDK. From the existing posts in the community regarding WLAN drivers, I am attaching below the portion of the boot script that is deviating from the proper one.

The Erroneous boot section:

[    4.978698] mmc1: card claims to support voltages below the defined range. These will be ignored.
[    5.012634] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
[    5.020416] mmc1: new SDIO card at address 0001
[    5.892578] kjournald starting.  Commit interval 5 seconds
[    5.900268] EXT3-fs (mmcblk0p2): using internal journal
[    5.905792] EXT3-fs (mmcblk0p2): recovery complete
[    5.912780] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[    5.920227] VFS: Mounted root (ext3 filesystem) on device 179:2.
[    5.926635] Freeing init memory: 212K
INIT: version 2.86 booting
Please wait: booting...
Starting udev
[    6.583374] udevd (755): /proc/755/oom_adj is deprecated, please use /proc/755/oom_score_adj instead.
[    7.425689] cfg80211: disagrees about version of symbol module_layout
[    7.435150] cfg80211: disagrees about version of symbol module_layout
[    7.593963] cfg80211: disagrees about version of symbol module_layout
[    7.624877] cfg80211: disagrees about version of symbol module_layout
Remounting root file system...

I waited and linux kernet got booted successfully. After booting linux, I tried to load the firmwares. It was showing as

Invalid module layout

I am new in this field. Please help me to overcome this problem.

Anindya

  • Hi Anindya,

    The errors you are seeing are wrt the building of the wl12xx drivers.

    Please visit: http://processors.wiki.ti.com/index.php/WL12xx_NLCP_Build_Instructions and follow the instructions there to build the wl12xx modules.

    Regards,
    Gigi Joseph.

  • Hi Joseph,

    I have built the wl12xx modules as per your suggestion.

    Should I just write the modified Root File System in the SD card for proper WLAN booting or I need to make any more changes in u-boot/uImage?

    If so, kindly provide me some suggestions regarding the same. Thanking you in advance,


    Anindya

  • Hi Anindya,

    Use the modified root file system. No need to modify u-boot, uImage. Once it boots up, check if the wl12xx modules are inserted.

    Regards,
    Gigi Joseph.

  • Hi Joseph,

    I booted with the modified Root File System. Now I am getting the following boot script.

    [    4.984252] mmc1: card claims to support voltages below the defined range. These will be ignored.
    [    5.021850] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
    [    5.030090] mmc1: new SDIO card at address 0001
    [   19.267791] kjournald starting.  Commit interval 5 seconds
    [   19.275665] EXT3-fs (mmcblk0p2): using internal journal
    [   19.281188] EXT3-fs (mmcblk0p2): recovery complete
    [   19.288360] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
    [   19.295806] VFS: Mounted root (ext3 filesystem) on device 179:2.
    [   19.302215] Freeing init memory: 212K
    INIT: version 2.86 booting
    Please wait: booting...
    Starting udev
    [   19.958709] udevd (756): /proc/756/oom_adj is deprecated, please use /proc/756/oom_score_adj instead.
    [   28.377044] Compat-wireless backport release: ol_R5.SP7.01
    [   28.382843] Backport based on wl12xx.git ol_R5.SP4.01-2-g1aa2c8e
    [   28.407958] cfg80211: disagrees about version of symbol module_layout
    [   28.425659] cfg80211: disagrees about version of symbol module_layout
    Remounting root file system...
    Caching udev devnodes
    Populating dev cachemv: cannot rename '/tmp/devices': No such file or directory
    ALSA: Restoring mixer settings...
    No state is present for card omap3evm
    Found hardware: "" "" "" "" ""
    Hardware is initialized using a generic method
    Configuring network interfaces... No state is present for card omap3evm
    [   50.346557] net eth0: ISR failed signaling test (IRQ 336)
    ifconfig: SIOCSIFFLAGS: No such device
    eth0      no wireless extensions.

    [   66.026245] net eth0: ISR failed signaling test (IRQ 336)
    ifconfig: SIOCSIFFLAGS: No such device
    done.
    Setting up IP spoofing protection: rp_filter.
    Fri Dec 23 00:34:00 UTC 2011
    INIT: Entering runlevel: 5
    Starting system message bus: dbus.
    Starting Dropbear SSH server: dropbear.
    Starting telnet daemon.
    Starting network benchmark server: netserver.
    Starting syslogd/klogd: done
    Starting thttpd.
    Starting PVR
    [   67.191009] pvrsrvkm: disagrees about version of symbol module_layout
    insmod: error inserting '/lib/modules/2.6.37/kernel/drivers/gpu/pvr/pvrsrvkm.ko': -1 Invalid module format
    [   67.223022] pvrsrvkm: disagrees about version of symbol module_layout
    FATAL: Error inserting omaplfb (/lib/modules/2.6.37/kernel/drivers/gpu/pvr/omaplfb.ko): Invalid module format
    [   67.254669] pvrsrvkm: disagrees about version of symbol module_layout
    FATAL: Error inserting bufferclass_ti (/lib/modules/2.6.37/kernel/drivers/gpu/pvr/bufferclass_ti.ko): Invalid module format
    BusyBox v1.13.2 (2011-12-23 00:31:29 IST) multi-call binary

    Usage: mknod [OPTIONS] NAME TYPE MAJOR MINOR

    Create a special file (block, character, or pipe)

    Options:
            -m      Create the special file using the specified mode (default a=rw)
    TYPEs include:
            b:      Make a block device
            c or u: Make a character device
            p:      Make a named pipe (MAJOR and MINOR are ignored)

    chmod: /dev/pvrsrvkm: No such file or directory
    [   67.485656] cmemk: disagrees about version of symbol module_layout
    FATAL: Error inserting cmemk (/lib/modules/2.6.37/kernel/drivers/dsp/cmemk.ko): Invalid module format
    [   67.570251] dsplinkk: disagrees about version of symbol module_layout
    FATAL: Error inserting dsplinkk (/lib/modules/2.6.37/kernel/drivers/dsp/dsplinkk.ko): Invalid module format
    [   67.594360] dsplinkk: disagrees about version of symbol module_layout
    FATAL: Error inserting lpm_omap3530 (/lib/modules/2.6.37/kernel/drivers/dsp/lpm_omap3530.ko): Invalid module format
    [   67.619323] sdmak: disagrees about version of symbol module_layout
    FATAL: Error inserting sdmak (/lib/modules/2.6.37/kernel/drivers/dsp/sdmak.ko): Invalid module format
    numid=49,iface=MIXER,name='HeadsetL Mixer AudioL1'
      ; type=BOOLEAN,access=rw------,values=1
      : values=on
    numid=46,iface=MIXER,name='HeadsetR Mixer AudioR1'
      ; type=BOOLEAN,access=rw------,values=1
      : values=on
    Simple mixer control 'Headset',0
      Capabilities: pvolume penum
      Playback channels: Front Left - Front Right
      Limits: Playback 0 - 3
      Mono:
      Front Left: Playback 1 [33%] [-6.00dB]
      Front Right: Playback 1 [33%] [-6.00dB]
    Starting Matrix GUI application.

    The same error is still coming in two lines in the boot log. Please help to overcome it.

    Also let me know the guidelines for setting up/calibrating/enabling the WLAN interface after proper booting is achieved.

    Thanking you,

    Anindya

  • Hi Anindya,

    This would again mean that the correct modules are not inserted - something to do with the build again.
    Please try to manually insert the modules and see if it helps.

    Regarding setting up/calibration/enabling the WLAN interface, everything is explained in the wiki - http://processors.wiki.ti.com/index.php/WL127x
    please go through it...

    Regards,
    Gigi Joseph.

  • Hi Joseph,

    While building the "wlxxbuild.sh" by the command "sudo ./wl12xx_build.sh all install" I got the following summary in the build log

    Please help me to nullify the warnings. Is it so that after these warnings are overcome, the wlan booting will happen properly?

    The summary of the build log is as follows:

    make[1]: Entering directory `/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk'
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/built-in.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/main.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat-2.6.38.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat-2.6.39.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/kstrtox.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat-3.0.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/cordic.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/crc8.o
    /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/crc8.c:17:1: warning: "pr_fmt" redefined
    In file included from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/printk.h:7,
                     from include/linux/kernel.h:20,
                     from include/linux/skbuff.h:17,
                     from include/linux/if_ether.h:125,
                     from include/linux/netdevice.h:29,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.29.h:5,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.h:24,
                     from <command-line>:0:
    include/linux/printk.h:161:1: warning: this is the location of the previous definition
    /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/crc8.c:17:1: warning: "pr_fmt" redefined
    In file included from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/printk.h:7,
                     from include/linux/kernel.h:20,
                     from include/linux/skbuff.h:17,
                     from include/linux/if_ether.h:125,
                     from include/linux/netdevice.h:29,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.29.h:5,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.h:24,
                     from <command-line>:0:
    include/linux/printk.h:161:1: warning: this is the location of the previous definition
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat_atomic.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/ethernet/atheros/built-in.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/ethernet/broadcom/built-in.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/built-in.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/main.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/event.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/tx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/rx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/ps.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/cmd.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/acx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/boot.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/init.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/debugfs.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/io.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/sdio.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/spi.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_spi.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_sdio.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_platform_data.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/built-in.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/main.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/cmd.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/io.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/event.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/tx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/rx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/ps.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/acx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/boot.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/init.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/debugfs.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/scan.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/testmode.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/sdio.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/spi.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_spi.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_sdio.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/built-in.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/built-in.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/main.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/status.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/sta_info.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/wep.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/wpa.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/scan.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/offchannel.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/ht.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/agg-tx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/agg-rx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/ibss.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mlme.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/work.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/iface.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rate.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/michael.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/tkip.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/aes_ccm.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/aes_cmac.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/cfg.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/spectmgmt.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/tx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/key.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/util.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/wme.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/event.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/chan.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/led.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/debugfs.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/debugfs_sta.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/debugfs_netdev.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/debugfs_key.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mesh.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mesh_pathtbl.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mesh_plink.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mesh_hwmp.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/pm.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/driver-trace.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rc80211_pid_algo.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rc80211_pid_debugfs.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rc80211_minstrel.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rc80211_minstrel_debugfs.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rc80211_minstrel_ht.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rc80211_minstrel_ht_debugfs.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/rfkill/built-in.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/core.o
    /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/core.c:7:1: warning: "pr_fmt" redefined
    In file included from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/printk.h:7,
                     from include/linux/kernel.h:20,
                     from include/linux/skbuff.h:17,
                     from include/linux/if_ether.h:125,
                     from include/linux/netdevice.h:29,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.29.h:5,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.h:24,
                     from <command-line>:0:
    include/linux/printk.h:161:1: warning: this is the location of the previous definition
    /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/core.c:7:1: warning: "pr_fmt" redefined
    In file included from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/printk.h:7,
                     from include/linux/kernel.h:20,
                     from include/linux/skbuff.h:17,
                     from include/linux/if_ether.h:125,
                     from include/linux/netdevice.h:29,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.29.h:5,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.h:24,
                     from <command-line>:0:
    include/linux/printk.h:161:1: warning: this is the location of the previous definition
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/sysfs.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/radiotap.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/util.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/reg.o
    /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/reg.c:36:1: warning: "pr_fmt" redefined
    In file included from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/printk.h:7,
                     from include/linux/kernel.h:20,
                     from include/linux/skbuff.h:17,
                     from include/linux/if_ether.h:125,
                     from include/linux/netdevice.h:29,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.29.h:5,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.h:24,
                     from <command-line>:0:
    include/linux/printk.h:161:1: warning: this is the location of the previous definition
    /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/reg.c:36:1: warning: "pr_fmt" redefined
    In file included from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/printk.h:7,
                     from include/linux/kernel.h:20,
                     from include/linux/skbuff.h:17,
                     from include/linux/if_ether.h:125,
                     from include/linux/netdevice.h:29,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.29.h:5,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.h:24,
                     from <command-line>:0:
    include/linux/printk.h:161:1: warning: this is the location of the previous definition
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/scan.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/nl80211.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/mlme.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/ibss.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/sme.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/chan.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/ethtool.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/mesh.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/debugfs.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/wext-compat.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/wext-sme.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/regdb.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/cfg80211.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/built-in.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/built-in.o
      Building modules, stage 2.
      MODPOST 8 modules
    WARNING: "cfg80211_probe_status" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_del_sta" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_notify_new_peer_candidate" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_cqm_pktloss_notify" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_report_obss_beacon" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_rx_spurious_frame" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_can_beacon_sec_chan" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_gtk_rekey_notify" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_ch_switch_notify" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_send_unprot_disassoc" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_roaming_status" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_send_unprot_deauth" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_send_intermediate_result" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_req_channel_switch" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_sched_scan_stopped" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_rx_unexpected_4addr_frame" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_sched_scan_results" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_find_vendor_ie" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx.ko] undefined!
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_sdio.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_sdio.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_spi.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_spi.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_sdio.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_sdio.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_spi.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_spi.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko
    make[1]: Leaving directory `/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk'
    make -C /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk M=/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless modules
    make[1]: Entering directory `/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk'
      Building modules, stage 2.
      MODPOST 8 modules
    WARNING: "cfg80211_probe_status" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_del_sta" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_notify_new_peer_candidate" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_cqm_pktloss_notify" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_report_obss_beacon" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_rx_spurious_frame" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_can_beacon_sec_chan" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_gtk_rekey_notify" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_ch_switch_notify" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_send_unprot_disassoc" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_roaming_status" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_send_unprot_deauth" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_send_intermediate_result" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_req_channel_switch" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_sched_scan_stopped" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_rx_unexpected_4addr_frame" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_sched_scan_results" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_find_vendor_ie" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx.ko] undefined!
    make[1]: Leaving directory `/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk'
    make -C /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk M=/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless "INSTALL_MOD_DIR=updates" "INSTALL_MOD_PATH=/home/ubuntu/targetfs" \
            modules_install
    make[1]: Entering directory `/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk'
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_sdio.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_spi.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_sdio.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_spi.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko
      DEPMOD  2.6.37
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/drivers/net/wireless/wl12xx/wl12xx.ko needs unknown symbol cfg80211_find_vendor_ie
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/wireless/cfg80211.ko needs unknown symbol trace_hardirqs_off
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/wireless/cfg80211.ko needs unknown symbol trace_hardirqs_on
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_sched_scan_results
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_rx_unexpected_4addr_frame
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_sched_scan_stopped
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_req_channel_switch
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_send_intermediate_result
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_roaming_status
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_ch_switch_notify
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_gtk_rekey_notify
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_can_beacon_sec_chan
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_rx_spurious_frame
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_report_obss_beacon
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_notify_new_peer_candidate
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_del_sta
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_probe_status
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/kernel/drivers/gpu/pvr/pvrsrvkm.ko needs unknown symbol trace_hardirqs_off
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/kernel/drivers/gpu/pvr/pvrsrvkm.ko needs unknown symbol trace_hardirqs_on
    make[1]: Leaving directory `/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk'

    Also please let me know what value should be set at the env-setup field BUILD_VERSION. Currently I have built the modules using the default value "r8".


    Thanking you in advance,

    Anindya


  • Hi Joseph,

    While building and installing the modules by the command "sudo ./wl12xx_build.sh all install" as recommended for first time installation, I got some warnings. I'm attaching the log below.

    make[1]: Entering directory `/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk'
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/built-in.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/main.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat-2.6.38.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat-2.6.39.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/kstrtox.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat-3.0.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/cordic.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/crc8.o
    /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/crc8.c:17:1: warning: "pr_fmt" redefined
    In file included from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/printk.h:7,
                     from include/linux/kernel.h:20,
                     from include/linux/skbuff.h:17,
                     from include/linux/if_ether.h:125,
                     from include/linux/netdevice.h:29,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.29.h:5,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.h:24,
                     from <command-line>:0:
    include/linux/printk.h:161:1: warning: this is the location of the previous definition
    /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/crc8.c:17:1: warning: "pr_fmt" redefined
    In file included from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/printk.h:7,
                     from include/linux/kernel.h:20,
                     from include/linux/skbuff.h:17,
                     from include/linux/if_ether.h:125,
                     from include/linux/netdevice.h:29,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.29.h:5,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.h:24,
                     from <command-line>:0:
    include/linux/printk.h:161:1: warning: this is the location of the previous definition
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat_atomic.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/ethernet/atheros/built-in.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/ethernet/broadcom/built-in.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/built-in.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/main.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/event.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/tx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/rx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/ps.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/cmd.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/acx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/boot.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/init.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/debugfs.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/io.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/sdio.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/spi.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_spi.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_sdio.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_platform_data.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/built-in.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/main.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/cmd.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/io.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/event.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/tx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/rx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/ps.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/acx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/boot.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/init.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/debugfs.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/scan.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/testmode.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/sdio.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/spi.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_spi.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_sdio.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/built-in.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/built-in.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/main.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/status.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/sta_info.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/wep.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/wpa.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/scan.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/offchannel.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/ht.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/agg-tx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/agg-rx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/ibss.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mlme.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/work.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/iface.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rate.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/michael.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/tkip.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/aes_ccm.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/aes_cmac.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/cfg.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/spectmgmt.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/tx.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/key.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/util.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/wme.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/event.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/chan.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/led.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/debugfs.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/debugfs_sta.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/debugfs_netdev.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/debugfs_key.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mesh.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mesh_pathtbl.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mesh_plink.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mesh_hwmp.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/pm.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/driver-trace.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rc80211_pid_algo.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rc80211_pid_debugfs.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rc80211_minstrel.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rc80211_minstrel_debugfs.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rc80211_minstrel_ht.o
      CC [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/rc80211_minstrel_ht_debugfs.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/rfkill/built-in.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/core.o
    /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/core.c:7:1: warning: "pr_fmt" redefined
    In file included from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/printk.h:7,
                     from include/linux/kernel.h:20,
                     from include/linux/skbuff.h:17,
                     from include/linux/if_ether.h:125,
                     from include/linux/netdevice.h:29,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.29.h:5,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.h:24,
                     from <command-line>:0:
    include/linux/printk.h:161:1: warning: this is the location of the previous definition
    /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/core.c:7:1: warning: "pr_fmt" redefined
    In file included from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/printk.h:7,
                     from include/linux/kernel.h:20,
                     from include/linux/skbuff.h:17,
                     from include/linux/if_ether.h:125,
                     from include/linux/netdevice.h:29,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.29.h:5,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.h:24,
                     from <command-line>:0:
    include/linux/printk.h:161:1: warning: this is the location of the previous definition
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/sysfs.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/radiotap.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/util.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/reg.o
    /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/reg.c:36:1: warning: "pr_fmt" redefined
    In file included from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/printk.h:7,
                     from include/linux/kernel.h:20,
                     from include/linux/skbuff.h:17,
                     from include/linux/if_ether.h:125,
                     from include/linux/netdevice.h:29,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.29.h:5,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.h:24,
                     from <command-line>:0:
    include/linux/printk.h:161:1: warning: this is the location of the previous definition
    /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/reg.c:36:1: warning: "pr_fmt" redefined
    In file included from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/printk.h:7,
                     from include/linux/kernel.h:20,
                     from include/linux/skbuff.h:17,
                     from include/linux/if_ether.h:125,
                     from include/linux/netdevice.h:29,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.29.h:5,
                     from /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/include/linux/compat-2.6.h:24,
                     from <command-line>:0:
    include/linux/printk.h:161:1: warning: this is the location of the previous definition
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/scan.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/nl80211.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/mlme.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/ibss.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/sme.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/chan.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/ethtool.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/mesh.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/debugfs.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/wext-compat.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/wext-sme.o
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/regdb.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/cfg80211.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/wireless/built-in.o
      LD      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/built-in.o
      Building modules, stage 2.
      MODPOST 8 modules
    WARNING: "cfg80211_probe_status" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_del_sta" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_notify_new_peer_candidate" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_cqm_pktloss_notify" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_report_obss_beacon" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_rx_spurious_frame" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_can_beacon_sec_chan" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_gtk_rekey_notify" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_ch_switch_notify" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_send_unprot_disassoc" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_roaming_status" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_send_unprot_deauth" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_send_intermediate_result" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_req_channel_switch" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_sched_scan_stopped" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_rx_unexpected_4addr_frame" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_sched_scan_results" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_find_vendor_ie" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx.ko] undefined!
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_sdio.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_sdio.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_spi.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_spi.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_sdio.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_sdio.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_spi.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_spi.ko
      CC      /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.mod.o
      LD [M]  /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko
    make[1]: Leaving directory `/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk'
    make -C /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk M=/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless modules
    make[1]: Entering directory `/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk'
      Building modules, stage 2.
      MODPOST 8 modules
    WARNING: "cfg80211_probe_status" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_del_sta" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_notify_new_peer_candidate" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_cqm_pktloss_notify" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_report_obss_beacon" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_rx_spurious_frame" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_can_beacon_sec_chan" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_gtk_rekey_notify" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_ch_switch_notify" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_send_unprot_disassoc" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_roaming_status" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_send_unprot_deauth" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_send_intermediate_result" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_req_channel_switch" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_sched_scan_stopped" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_rx_unexpected_4addr_frame" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_sched_scan_results" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko] undefined!
    WARNING: "cfg80211_find_vendor_ie" [/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx.ko] undefined!
    make[1]: Leaving directory `/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk'
    make -C /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk M=/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless "INSTALL_MOD_DIR=updates" "INSTALL_MOD_PATH=/home/ubuntu/targetfs" \
            modules_install
    make[1]: Entering directory `/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk'
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/compat/compat.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_sdio.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl1251/wl1251_spi.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_sdio.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/drivers/net/wireless/wl12xx/wl12xx_spi.ko
      INSTALL /home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/compat-wireless/net/mac80211/mac80211.ko
      DEPMOD  2.6.37
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/drivers/net/wireless/wl12xx/wl12xx.ko needs unknown symbol cfg80211_find_vendor_ie
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/wireless/cfg80211.ko needs unknown symbol trace_hardirqs_off
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/wireless/cfg80211.ko needs unknown symbol trace_hardirqs_on
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_sched_scan_results
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_rx_unexpected_4addr_frame
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_sched_scan_stopped
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_req_channel_switch
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_send_intermediate_result
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_roaming_status
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_ch_switch_notify
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_gtk_rekey_notify
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_can_beacon_sec_chan
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_rx_spurious_frame
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_report_obss_beacon
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_notify_new_peer_candidate
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_del_sta
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/updates/net/mac80211/mac80211.ko needs unknown symbol cfg80211_probe_status
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/kernel/drivers/gpu/pvr/pvrsrvkm.ko needs unknown symbol trace_hardirqs_off
    WARNING: /home/ubuntu/targetfs/lib/modules/2.6.37/kernel/drivers/gpu/pvr/pvrsrvkm.ko needs unknown symbol trace_hardirqs_on
    make[1]: Leaving directory `/home/ubuntu/ti-dvsdk_dm3730-evm_04_03_00_06/psp/linux-2.6.37-psp04.02.00.07.sdk'


    Is it so that these warnings are creating the errors in the boot log?If so please help me to overcome these warnings.

    Also, please let me know the value to be entered in the 'BUILD_VERSION' field in the 'setup-env' file. So far I have built keeping the default value of "r8" as in the file 'setup-env.sample".

    In my board, the used clock frequency for the Fast clock of the processor is 26MHz. Under this condition, what should be the setting for ".board_ref_clock" for the Wireless module 'wl12xx'

    Thanking you in advance,

    Anindya

  • Anindya,

    Those warnings are not good... I have not seen them before.

    I think one of the values you have put in setup-env is not correct... Just try "wl12xx_build.sh all build" and see if all the modules get generated (without the warnings).

    BUILD_VERSION should be "r5" in your case.

    Regarding your other questions, please refer to the wiki page I provided earlier.

    Regards
    Gigi Joseph.

  • Hi,

    Thank you for your nice suggestion. I made an error in putting the proper directory for installing the modules. Now I put the modules in rootfs/usr/bin and rebooted the board and WLAN is booting up properly. I am able to power up and power down it from processor.

    But, I am having problem in Tx/Rx/Calibration of the module. Please check my post in the thread named "wl1271 calibration problem" in "WiLink™ WiFi + Bluetooth Forum".

    Thanking you again,

    Anindya