I am using the WL1273 on an OMAP L138 cpu. 

 

I am using the driver from the "omap" git tree.  It appears to be working;  I can down load firmware

but I don't have a valid "calibration file".

 

If I had an OMAP3530 I would use the evm release and run "wlan_cu", but I can not do this with

an L138 cpu as the wiwlan driver does not support the L138 - it only supports the 3530.

 

I can not use  omap git tree driver because it does not support the private ioctl calls which wlan_cu uses.

 

Is there some documentation for the "nvs_map.bin" file?  looking at the sources it appears to be

a simple "tlv" style binary file but which tags are required by the firmware does not seem to be documented

anywhere.

 

I'd like to make a simple "default" file which I can use for bench testing.  I have looked everywhere and

found nothing.  Some docs on the contents of the file would help.

 

ps: I understand the evm does not support the L138 but there must be some support somewhere for

people who are using different cpus...