• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Low Power RF & Wireless Connectivity » WLAN Applications Forum » All Tags » WLAN
Share
Low Power RF & Wireless Connectivity
  • Forums
  • Announcements
  • Files
  • E2E Wiki

Browse by Tags

Low Power RF & Wireless Connectivity

Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
WLAN
  • 1271
  • 1273
  • 802.11
  • Android
  • bluetooth
  • BT
  • devkit
  • OMAP 3530
  • OMAP WL1271
  • sdio
  • Wi-Fi
  • WIFI
  • WIFI RELATED
  • wireless
  • WL1271
  • WL1271 Bluetooth
  • WL1271 Bluetooth omap3evm
  • wl1271 driver
  • WL1271 module
  • WL1271 module start WLAN
  • WL1271 port
  • WL1271 Power Save
  • wl1271 wifi
  • WL1273
  • wlan_cu
Related Posts
  • Forum Post: Re: Wi-Fi Ad-hoc network using WL1271

    Nestor49613 Nestor49613
    Thank you very much for the answer Sinoj. Do you know if it is possible to request a specific security (eg. WEP, WPA) to be used for the created Ad-hoc network and to specify the key/passphrase to be used for accessing that ad-hoc network? Best regards, Nestor
    on Jul 29, 2010
  • Forum Post: Wi-Fi Ad-hoc network using WL1271

    Nestor49613 Nestor49613
    Hi all, I'm trying to find out if there is ad-hoc Wi-Fi network support in WL1271. I can see that there is an option to connect to an existing ad-hoc network in the CLI application. However I couldn't find a way to create an ad-hoc network that other WL1271 chips would connect to. Could...
    on Jul 28, 2010
  • Forum Post: Re: WL1271 Setup Guide, wlan_Init.sh script missing from supplied software.

    hdp hdp
    Hello, I am using the wl1271_wlan.sh to run the demo. The WL1271 DEMO MAIN MENU comes up after running the script. When I choose DEMO OPTION 1 for Wireless Demo I get the following error. Insert: "sdio.ko" module failed ERROR: Module sdio does not exist in /proc/modules Does...
    on Nov 16, 2010
  • Forum Post: Re: wl1271 chip ID read operation fails

    Sanjay Kumar42857 Sanjay Kumar42857
    Hi Andrea, There may be issue for MMC 3 communication. To resolve this problem can you follow the below procedure? 1. Build the WiLink driver for OMAP35x platform and it will generate "sdio.ko", "bmtarce.ko", "tiwlan_drv.ko" and "testsdio.ko". 2. Upload...
    on Nov 26, 2010
  • Forum Post: Re: WL1271 driver for uC/OS-II

    Matt Kurtz Matt Kurtz
    Dhanesh, We do not have a WLAN driver for uC/OS-II. If you want to try and make it work on your own, there is a Linux WLAN driver for 1271 using the mac80211 open source kernel solution. The driver is called wl12xx and it is maintained as part of the linux-wireless community. Here is a basic wiki...
    on Feb 3, 2011
  • Forum Post: Periodic issue with LSR wl1271 module

    Guillaume RAMOUSSE Guillaume RAMOUSSE
    I'm working on an OMAP3530 board from M2M solution and a module from LSR based on the 1271 chip. I encounter two issues, the first one is about the sdio speed, when it's set at 26MHz it works 1 on a 100 times, I have almost always error messages after firmware download. When I set the frequency...
    on Jan 30, 2011
  • Forum Post: XCC_MODULE_INCLUDED define

    none none62284 none none62284
    Hi, I would like to learn something about the XCC_MODULE_INCLUDED define. It is related to the WPA Enterprise but could any one tell me when is it used and what does it mean? Regrads, Krzysztof
    on Feb 28, 2011
  • Forum Post: Re: Not connect in case of fixed transmission rate

    Alon Srednizki Alon Srednizki
    Hi, Please refer to our wiki in the following link: http://processors.wiki.ti.com/index.php/ARM_Processor_Wireless_Connectivity_FAQ#How_configure_supported_rates.3F It explains about how to configure\mask supported rates, for doing the same with basic rates just replace "Supported" with...
    on Mar 21, 2011
  • Forum Post: Re: WL1271 Information

    ajit basarur ajit basarur
    Hi, I have following queries w.r.t WL1271 device From the WL1271 daughter card provided to OSK Rev-G board, I could observe that there are three connectors provided for antenna connectivity to WL1271 chip and out of which one of the connector is routed to antenna on-board. My questions are 1...
    on Mar 22, 2011
  • Forum Post: Re: Questions on triggered scan behaviour

    Saurabh Narang Saurabh Narang
    Tracking scan has minimum dwell time set to 500msec and discovery and immediate scan have minimum dwell time set to 1sec. WiFi device stays on that scan channel for at least that duration . This is the reason why you noticed 500mse delay in channel switch in normal scenario and 1 sec delay when AP count...
    on Apr 2, 2011
  • Forum Post: Re: Not connect in case of fixed transmission rate

    Alon Srednizki Alon Srednizki
    Hi, If you would like to use a fixed rate, then yes, you need to set it as a basic rate too. I wouldn't say that it's a specification of WL1271 per say, but a general behavior of 802.11. Thanks, Alon.S
    on Apr 11, 2011
  • Forum Post: Re: How to set the Maximum Tx Power for WL1271/3

    Alon Srednizki Alon Srednizki
    Hi Noah, TxPower may differ from 11b, 11g & 11a. In general our solution supports 11d which handles the power limits per country (country, channel, band). If you are working with AP that doesn't support 11d then as a station you don't have to support all this restrictions (we are a passive...
    on Apr 11, 2011
  • Forum Post: how to get the TI wlan chip ..wl1281's driver for kernel ->2.6.38.4

    tristan von tristan von
    Hi, I am trying to tune a wi-fi Module which wl1281 in it . but , i just find the driver of wl1271 do you have release the source for wl1281 ,yet ? where can i download it ? many many thanks ~!
    on Apr 27, 2011
  • Forum Post: Re: wl1273 download firmware errorS

    xiang71740 xiang71740
    Hi Eyal, The module we are using is from Murata.It works well on TI DM365 with the kernel source and WiLink package provided by Murata.Now i need to port that to our IPNC sys.The SDIO driver is using DM365 SDIO1 with DMA (Supporting 4-bit mode).(It was ported from OMAP2430 i think). The driver...
    on Jun 15, 2011
  • Forum Post: Re: WL1271 RSSI Max value

    Alon Srednizki Alon Srednizki
    Hi Sivaram, RSSI max value is indeed limited by SW to -45 (the HW has no issues receving stronger packets). I'm not sure to what percentage table you are referring to. However, since our RF sensitivity is -89dBm a possible conversion for GUI perspective can be between -45 (100%) to -89(0%)...
    on Jun 26, 2011
  • Forum Post: wl1273 download firmware errorS

    xiang71740 xiang71740
    Hi ALL, We are using the WLAN module with WL1273,when downloading the firmware.bin,it hangs with "Starting to download firmware..." ********************************************************** # ./sta_run davinci-mmc davinci-mmc.0: Supporting 4-bit mode davinci-mmc davinci-mmc.0: Using...
    on Jun 13, 2011
  • Forum Post: Trouble Getting Custom Board with WL1271 to Initialize

    Chris R Chris R
    We have a custom board with a WL1271 (in a TiWi01-R2 module) that we are having trouble initializing. We have a single GPIO that controls both our Vbat (@ 3.3V) and Vio (@ 1.8V) power rails to the module. The power-up sequence diagrams all show Vbat coming up before Vio. Is there any requirement for...
    on Aug 9, 2011
  • Forum Post: Re: AM1808 EVM WEP setup

    BrandonAzbell BrandonAzbell
    The path to use will depend on which Linux Software Development Kit you are starting with. The latest Linux SDK is available from the following link below. http://focus.ti.com/docs/toolsw/folders/print/linuxezsdk-sitara.html Select the LINUXEZSDK-AM18X option. The Open Source Wireless driver...
    on Aug 28, 2011
  • Forum Post: Re: devkit2.2/rowboat DM3730 and ti wl1271 drivers using MMC3 interface

    Andrew Watts82915 Andrew Watts82915
    Eyal, I have a beagleboard XM with the beagletoys wl1271 adapter board attached. I am currently using the 2.3.4 dev kit for android (i have also pulled the latest from git). I have tried to integrate the driver into the beagleboard build system but haven't had much luck. All of the pieces seem...
    on Aug 30, 2011
  • Forum Post: Re: wl1273 can't find any AP and can't connect .

    Alon Srednizki Alon Srednizki
    Hi Lynn, Did you run TxBIP on your device? Please refer to our wiki for the exact information: http://processors.wiki.ti.com/index.php/ARM_Processor_Wireless_Connectivity_FAQ#How_can_I_run_Tx_BIP_.28WLAN_Calibration.29.3F Thanks, Alon.S
    on Sep 12, 2011
  • Forum Post: External Calibration WL127x module

    Igmar Hernandez Igmar Hernandez
    Hi I have some doubts related to the external calibration process for the WL127x module. I know that there are 3 types of load during calibration: - Loop back - Internal FEM load - External Load (using the antenna) I also know that for Bip Calibration the load is either internal or external depending...
    on Oct 27, 2011
  • Forum Post: WiFi power control

    Zory Marantz Zory Marantz
    Hi All, I'm setting up a research project that requires me to control the power output of a WiFi node. specifically, I'm testing out an algorithm that measures received signal strengths, does some number crunching, and then modifies the output power per some specification. Ideally, I would...
    on Nov 15, 2011
  • Forum Post: Re: am3517 som-m2 bluetooth

    HONGSEN LI HONGSEN LI
    I am using AM3517 SOM-M2,i want to make bluetooth work.I just do according to the document in "OMAP35x Wireless Connectivity Getting Started Guide",but i can not get "WiLink_L23.i3.6.tar.gz" from " http://dev.omapzoom.org " could you give me a link to get "WiLink_L23...
    on Dec 19, 2011
  • Forum Post: AM1808-WL1271 web-based sample codes issue.

    Carl Liu Carl Liu
    Hi, We will use WL1271 Wifi module on AM1808 development kit. Can we set Wifi configuration by web page? Does TI have AM1808-WL1271 web-based sample codes to reference? Sincerely, Carl
    on Jan 19, 2012
  • Forum Post: Does anyone know if the following configurations can be done with MCP CLI Tool?

    Igmar Hernandez Igmar Hernandez
    Hi Does anyone know if the following configurations can be done with MCP CLI Tool? Place the radio in Continuous Transmit mode with pseudo-random modulated packets Place the radio in Continuous Waveform mode with non-modulated packets Place the radio in Continuous Receive mode and report...
    on Aug 27, 2011
12
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use