Hi,
Following a little along the lines of Gary Siu (CC85XXDK Headset Noise), I have also experienced unacceptable noise with the Demo as supplied, and with +20 dB of input offset added, which may due to incorrect set-up on my part, for which I ask advice.
Using the example files, 'Bi-directional Demo', I conducted two tests, one with the Example 'as is', and a second with +20 dB offset added to both Master and Slave inputs (previously +6 dB for M, now +26 dB, and previously 0 dB for S, now +20 dB). Both test results were similar, with all output signal and noise levels increased by about 20 dB, which were more noticeable and easier to measure.
I will only provide the 20 dB offset tests in the Post, because they are more relevant as I have to have at least 20 dB and possibly +40 dB amplification more than that provided in the Demo. This is necessary because I will be using electret microphones (Sensitivities -50 to -40 dB, with Ref 0 dB = 1V/Pa; where 1 Pa = 94 dB SPL) in noisy environments. Note that this Sensitivity range results in 3 to 10 mV (RMS) signal outputs into the input stage of the AIC3101; equivalent to around 95 dB speech into a close talking, noise cancelling microphone.
For input, I used a sine wave at 1 kHz, and 1.5 mV(RMS) i.e. -54 dBm as input. For convenience, I have used "S" for Slave, and "M" for Master; and "L" for Left and "R" for Right channels:
PART A - S as input and M as Output
1. Signal into S, L Line In or L mic in; M produces medium volume in L & R outputs, with bad Medium Frequency noise (MF) - see attached noise file "1-M-Bi-Di +20 dB Sig A"
2. Signal into S, R Line In or R mic in; M produces no output as expected
3. No Signal into S, L Line In or R mic in; M produces MF noise; see attached noise file "2-M-No Sig A"
4. No Signal into S, L Line In or R mic in; M produces MF noise and various hum components up to 400 Hz when finger touches S phono input socket earths; see attached noise file "3-M Finger on earth"
5. No Signal into S, L Line In or R mic in; M produces significantly reduced MF noise when hand is held within 3 to 5 mm of S RF PCB, which suggests induced RF or clock noise.
PART B - M as input and S as Output
1. Signal into L Line In or L mic in; S produces L signal without noise; refer to attached noise file "4-S-Sig A"
2. Signal into R Line In or R mic in; S produces R signal without noise; refer to attached noise file "4-S-Sig A"
I have repeated these tests on 4 different CC85XX DK boards and a number of RF PCBs, with similar results to each other - there is some variation, with some boards being slightly noisier than others.
Attached also please find the Project and Configuration Files used for the tests - Only the Configurator Volume panel was changed to add +20 dB offset to both M and S inputs.
Whilst TI questioned Gary Siu's need to have +45 dB offset, and advised him to change the mic bias conditions, the fact is that more amplification is required than that provided in the Bi-Directional Demo. I appreciate that raising input amplification will increase the noise floor, but this is no problem for Part B above, but is a major problem for Part A above.
Could you please advise me what I am doing incorrectly.
Regards,
Geoff Pickford
Hi Kristoffer.
Have tested the three configurations, and all come out really good, very similar to the test results I posted yesterday. We will now study them to make sure we can create other successful configurations.
I tried reseting the 'audio device customisation' on your 3 examples, and found two of them to do exactly as you said in your last post.
However, your 'bi_directional_2slaves_micInputs' did not. The two lists below show only those registers changed:
Before Reset:
OFF to SR-SWITCHw 30 2A 60 # Pop reduction, output drivers delayed 100 msw 30 11 0F # Single-ended MIC2 in L, gain 0 dbw 30 12 F0 # Single-ended MIC2 in R, gain 0 db
INACTIVE to LOW-POWERw 30 19 80 # Enable mic bias 2.5Vw 30 13 FC # Left ADC poweredw 30 16 FC # Right ADC powered
LOW-POWER to ACTIVEOK
ACTIVE to LOW-POWEROK
LOW-POWER to INACTIVEw 30 0F 80 # Mute left ADC PGAw 30 10 80 # Mute right ADC PGAw 30 19 00 # Disable mic biasw 30 13 F8 # Left ADC unpoweredw 30 16 F8 # Right ADC unpowered
After Reset:
OFF to SR-SWITCHw 30 13 80 # Fully-differential line in L 1, gain 0 db, left ADC unpoweredw 30 16 80 # Fully-differential line in R 1, gain 0 db, right ADC unpoweredw 30 2A 60 # Pop reduction, output drivers delayed 100 ms
INACTIVE to LOW-POWERw 30 00 00 # Select register page 0w 30 13 84 # Fully-differential line in L 1, gain 0 db, left ADC poweredw 30 16 84 # Fully-differential line in R 1, gain 0 db, left ADC powered
LOW-POWER to INACTIVEw 30 13 80 # Fully-differential line in L 1, gain 0 db, left ADC unpoweredw 30 16 80 # Fully-differential line in R 1, gain 0 db, right ADC unpowered
In other words, resetting changed the registers from mic inputs to RCA inputs, despite the fact that I had previously completely deleted all TI files and Configurator, and re-installed.
I tried another computer (both running VMWare Fusion on Macs running OS 10.7.4), and the same configuration did the same thing. Further, 'bi_directional_mono_micInputs' changed, but only the order of several of the registers as they appeared on the page, but not the contents.
I deleted all TI files and Configurator on the second Mac, and it then behaved like the first Mac.
QUESTION: Could you please tell me how this may have occurred, because to me it is an unknown factor that is likely to cause problems in the future?
Hi Geoff,
Great that the configurations worked well!
The reason that the codec settings for "bi_directional_2slaves_micInputs" changes when you press "Reset all" is because I have modified the sequences inside the Audio device customization panel to match your requirements. Let me explain:
When custom setup of the audio device is disabled the settings in the ppwadd file is used. When custom setup is enabled the settings inside the Audio device customization panel have presidence over the ppwadd file. If you press "Reset all" the configurator will read from the ppwadd file and copy these settings into the sequences in the Audio device customization panel.
A rather confusing thing (which will be fixed in the next configurator release) is the fact that many of the example projects have old (non-ideal) saved settings that will apply if custom setup of the audio device is enabled. For example if you open the example project "CC85XXDK - Wireless Headset" you will see that custom setup of the audio device is disabled for both M and S. So-far everything is ok, and this example works as it should. The settings in the ppwadd file is now used. But if you enable custom setup for the master, and then click the Audio device customization panel you will see old saved settings. These saved settings are part of the device configuration ("cc85xxdk_demo_analog_input_bi_directional_master.ppwexcfg") and has nothing to do with the ppwadd file. They have now presidence over the ppwadd file. If you now press "Reset all" you will see that the settings change, because "Reset all" reads the ppwadd file and copy these settings into the Audio device customization panel.
In the following projects bi_directional_stereo_RCA_customSetupEnabled and bi_directional_mono_micInputs I have enabled custom setup and pressed "Reset all" (because you requested me to) so that you could see the configurations. I could have just disabled the custom setup and it would have been equivalent. So why you see changes in Mac OS is very strange!! Are you certain that you used the same configurator versions on your windows machine and your Mac?
Regards
Kristoffer
-- Thank you for clicking Verify Answer if this answered your question!
Hello Kristoffer,
Thanks for your helpful description in your Aug 2 Post. This and other information TI has provided has assisted me in creating successful Projects, albeit a bit laborious, and I would like to list the detailed description of this creation to see if it can be improved;
Question 1: Your process looks fine.
Question 2: You are right. If you want to make changes to an allready existing audio device definition, and you want this change to apply every time you press the reset all button, you must do this change within the audio device definition file (.ppwadd). However, instead of making changes directly in the files that comes together with the download of the configurator, we recommend to make a copy of the device definition file you want to change and save this copy in the following folder:
C:\Documents and Settings\<user>\My Documents\Texas Instruments\PurePath Wireless Configurator\audio_devices\
If the name tag (inside the definition) is identical to a name tag in an allready existing audio device definition the user generated audio device definition overrides the installed (original) one, and this will be marked with a # in the audio device list. For more info see the" Audio Device Definition Files" chapter in the configurator help system under the sub chapter "File Handling".
Two features in the configurator that might be useful to you:
"Copy existing..." - This is a button in the Project panel that is handy if you want to create a device configuration that will be only slightly different than an allready exixting device configuration.
"Import settings from other device configuration" - This button is located next to the "Save" button. Pressing this button will copy the current sub panel of an allready existing device configurations.
Best regards
Will do all you have suggested.
However, what if you want different Codec settings for different configurations in the one project, eg Line Input for M and Microphone inputs for S, or even more so, very different audio paths through the Codec for each of the 3 configurations. It appears to me that the .ppwadd changes are global. Is it possible to define this in the ,ppward file - which to me seems magically to call on specific Application Roles, each of which can be different, but not sure how to use it for my question.
Also, I would value comments on Question 3 (re noise) of my post of Aug 5.
Finally, do you have any PCB layouts of the CC85XX using a chip antenna, or even third party sources of these? if not, having no experience with RF design, is it possible to use the existing PCB layout (used in the CC85XX DK) and simply replace the inverted F antenna with a chip - both seem to need a 50 ohm feed.
Many thanks,
Geoff,
My comments to item 3 - there will be power-pulling with frequency = 1/timeslot. The higher RF output power on the board the bigger the pull. This has to do with the fact that a CC85xx will draw ╠~10mA with the radio off and ~30mA with the radio on (standalong at ~+5 dBm outputpower). With the CC2590 the difference between off and on can be twice as much. Proper care with regards to layout have to be taken to prevent this from being picked up by the audio paths. For your setup that has a ADC at the slave side and DAC at the master side (or visa versa) this pulling can be picked up at both sides.
We spent a significant amount of effort on this on both our standard DK and the DK-HEADSET to minimize the effect, but amplify the signal enough (input volume offset for the slave/ADC and PC/Recorded input gain for the master/DAC) and you will be able to find traces of this. Remember that to be able to see this for the plot i posted I had to turn the input gain in my laptop to maximum. Without doing this I was not able to detect anything.
Layout techniques to minimize power pulling includes:- splitting of ground planes (Audio and RF)- star-routing of power (GND and VCC)- separate power regulators (Audio and RF) with good power supply rejection ratio- good decoupling placed as close to circuits as possible
Best regards, Kjetil
--PS. Thank you for clicking Verify Answer if this answered your question!
Kjetil,
It certainly appears that your team achieved a really good result in respect to noise in terms of circuit and OCB design.
As indicated in my previous post, my colleague and I spent a fair part of today trying to put Kristoffer's suggestions into practice - without success due to two main problems. We had previously duplicated the aic3101.ppwadd file and a stereo and mono version of the .ppward files, and stored them as instructed inside the appropriated sub-directories in the 'My Documents' Directory. These files were modified by changing the internal names etc so as to be consistent with the .ppwcfg files.
It did not matter what we did, but the Configurator did not recognise the new .ppward files, because they did not cause the .ppwcfg files to even specify that they were M or S files etc.
We then changed the duplicate aic3101.ppwadd file and found this also was not effective in passing on its information to the .ppwdcfg files. Even small 'comments' changes were not passed on.
Worse than this, when we Reset All, the original version of the aic3101 file showed in the Customization panel, EVEN WHEN we deleted both the original and modified files. In other words, there was no aic3101.ppwadd file in any directory.
QUESTION 1. Any thoughts on getting the project to recognise modified .ppward files? For example, can you please list essential parts of these files that have to be consistent with other files such as .ppwcfg and .ppward files?
QUESTION 2. Any ideas where the Configurator is finding the deleted aic3101.ppwadd files? Same thing happens when we insert Default. It almost appears as if there is another aic3101.ppwadd file somewhere embedded in the Configurator.
QUESTION 3. (already posted) Do you have any PCB layouts of the CC85XX using a chip antenna, or even third party sources of these? if not, having no experience with RF design, is it possible to use the existing PCB layout (used in the CC85XX DK) and simply replace the inverted F antenna with a chip - both seem to need a 50 ohm feed.
Thanks again for being so patient - I am hoping the frequency of my questions will soon drop to just about nothing.
QUESTION1:
I'm not sure if I understand your question or problem. Could you please elaborate on what you are trying to do? If it helps I have attached a modified ppward file that should be recognized by the configurator. Place this in the "application_roles" folder under My Documents, and you should see it under "MASTER - Upstream audio" in the configurator. The name will be "MODIFIED Stereo output base station". An important part of the <name> tag is the Slave/ or Master/ prefix in the start of the name.
<name>Master/MODIFIED Stereo output base station</name>
QUESTION 2:
The only place the configurator looks for .ppwadd-files is in the "audio_devices" folder in the install folder and the "audio_devices" folder in My Documents. I tried to remove the aic3101.ppwadd file from the install folder (I don't have any in my My documents folder), and as a result the example project "CC85XXDK - Preloaded Demo" gives an error message in the Audio Interface panel because no audio device is selected. The drop down list doesn't have an option for selecting aic3101. The only possible explanations I can come up with to explain why you still see aic3101 in the list are:
- Maybe you have (by a mistake) modified the name tag inside some of the other ppwadd-files. For example if you open your aic3204.ppwadd file in an editor you could maybe see that the name tag is aic3101.
- Maybe you are looking too fast in the drop down list and that you are mistaking adc3101 to be aic3101. I have done this a few times...
- Maybe you have deleted your aic3101 files while the configurator is running and expecting to see the impact of this delete immediately. You have to close and reopen the configurator in order to see the effect of deleting ppwadd-files.
The magic you are referring to is something we have talked about earlier. There are several filters in the ppwadd-files in order to set up different i2c sequences depending on the application role selected. For examplein the aic3101.ppwadd you find:
On line 57:
<cfg_sequence_filter_spec name="mic_input"> <application_role_list>Master/Mono headset,Slave/Mono headset,Slave/Stereo headset,Slave/Mono microphone,Slave/Stereo microphone</application_role_list> </cfg_sequence_filter_spec>
These lines have the following meaning: If some of the listed application roles are selected we have what we have called "mic_input". Further down in the file on line 82 we see:
-{mic_input w 30 13 80 # Fully-differential line in L 1, gain 0 db, left ADC unpowered w 30 16 80 # Fully-differential line in R 1, gain 0 db, right ADC unpowered -} +{mic_input w 30 11 0F # Single-ended MIC2 in L, gain 0 db w 30 12 F0 # Single-ended MIC2 in R, gain 0 db +}
This means that if the application role selected is one of the following:
Master/Mono headset, Slave/Mono headset, Slave/Stereo headset, Slave/Mono microphone, Slave/Stereo microphone
we have mic_input and the i2c sequence that will be applied is
w 30 11 0F # Single-ended MIC2 in L, gain 0 dbw 30 12 F0 # Single-ended MIC2 in R, gain 0 db
If any other appliaction role is selected we don't have mic_input and the i2c sequence that will be applied is
w 30 13 80 # Fully-differential line in L 1, gain 0 db, left ADC unpoweredw 30 16 80 # Fully-differential line in R 1, gain 0 db, right ADC unpowered
QUESTION 3:
Unfortunatelly we don't have any ref designs using chip antennas. But simply copy TI's ref design all the way to the PCB antenna (you can skip the zero ohm and the placeholder for the shunt component), and continue with the ref design for the chip antenna (they often come with some recommended external components). Just make sure the antenna is a 50 ohm antenna and designed to operate in the 2.4 GHz band.
To your question:
"However, what if you want different Codec settings for different configurations in the one project, eg Line Input for M and Microphone inputs for S, or even more so, very different audio paths through the Codec for each of the 3 configurations."
Then I suggest to modify this in the Audio device customization panel inside the configurator for each of the device configurations.
-Kristoffer