Hi,
Following a little along the lines of Gary Siu (CC85XXDK Headset Noise), I have also experienced unacceptable noise with the Demo as supplied, and with +20 dB of input offset added, which may due to incorrect set-up on my part, for which I ask advice.
Using the example files, 'Bi-directional Demo', I conducted two tests, one with the Example 'as is', and a second with +20 dB offset added to both Master and Slave inputs (previously +6 dB for M, now +26 dB, and previously 0 dB for S, now +20 dB). Both test results were similar, with all output signal and noise levels increased by about 20 dB, which were more noticeable and easier to measure.
I will only provide the 20 dB offset tests in the Post, because they are more relevant as I have to have at least 20 dB and possibly +40 dB amplification more than that provided in the Demo. This is necessary because I will be using electret microphones (Sensitivities -50 to -40 dB, with Ref 0 dB = 1V/Pa; where 1 Pa = 94 dB SPL) in noisy environments. Note that this Sensitivity range results in 3 to 10 mV (RMS) signal outputs into the input stage of the AIC3101; equivalent to around 95 dB speech into a close talking, noise cancelling microphone.
For input, I used a sine wave at 1 kHz, and 1.5 mV(RMS) i.e. -54 dBm as input. For convenience, I have used "S" for Slave, and "M" for Master; and "L" for Left and "R" for Right channels:
PART A - S as input and M as Output
1. Signal into S, L Line In or L mic in; M produces medium volume in L & R outputs, with bad Medium Frequency noise (MF) - see attached noise file "1-M-Bi-Di +20 dB Sig A"
2. Signal into S, R Line In or R mic in; M produces no output as expected
3. No Signal into S, L Line In or R mic in; M produces MF noise; see attached noise file "2-M-No Sig A"
4. No Signal into S, L Line In or R mic in; M produces MF noise and various hum components up to 400 Hz when finger touches S phono input socket earths; see attached noise file "3-M Finger on earth"
5. No Signal into S, L Line In or R mic in; M produces significantly reduced MF noise when hand is held within 3 to 5 mm of S RF PCB, which suggests induced RF or clock noise.
PART B - M as input and S as Output
1. Signal into L Line In or L mic in; S produces L signal without noise; refer to attached noise file "4-S-Sig A"
2. Signal into R Line In or R mic in; S produces R signal without noise; refer to attached noise file "4-S-Sig A"
I have repeated these tests on 4 different CC85XX DK boards and a number of RF PCBs, with similar results to each other - there is some variation, with some boards being slightly noisier than others.
Attached also please find the Project and Configuration Files used for the tests - Only the Configurator Volume panel was changed to add +20 dB offset to both M and S inputs.
Whilst TI questioned Gary Siu's need to have +45 dB offset, and advised him to change the mic bias conditions, the fact is that more amplification is required than that provided in the Bi-Directional Demo. I appreciate that raising input amplification will increase the noise floor, but this is no problem for Part B above, but is a major problem for Part A above.
Could you please advise me what I am doing incorrectly.
Regards,
Geoff Pickford