Hi Guys,
Is there any manuall or help file on using the PurePathWirelessProgrammer.exe program command line tool?
I wish to use it for mass programming on the production floor.
Thank you,
Nir.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Guys,
Is there any manuall or help file on using the PurePathWirelessProgrammer.exe program command line tool?
I wish to use it for mass programming on the production floor.
Thank you,
Nir.
Hi Nir,
It's documented within the tool itself (launch it in a command window).
It's a very basic tool - you will need the ID of the CC debugger you are using. This can be found with the configurator.
This functionality is also built into the PurePath Wireless Commander tool:
http://www.ti.com/tool/purepath-wl-cmd
Regards,
Kjetil
I now know what happened. I tried copying the exe and its dll files to another directory and run
it from there and it did not run well. Must i run the command line in the same directory as the PPWC is installed?
Nir.
Hi Nir,
if you have not added the path of the folder to your Environment Variables in windows, you must to run the .exe from install directory using the command line. Do a quick search for e.g. path and environment variables in windows to find more about how to be able to run this .exe from "another directory".
Best regards,
Johan