I'm trying to build a system with a CC8520. I have a purepath wireless audio EB 1.2 with a CC8531 to work with.
- Will my slave 8520 link with the master 8531 eval board?
- I loaded "CC85XXDK Preloaded Demo" SLAVE onto my 8520 board and it programmed successfully. However, the status LED for the radio is really dim and doesn't seem to respond to what I program it to be (whether that's 50% on/off or 90%/10%). I've tried both 1k resistor and 560ohm resistor in line with my LED. The 8531 status LED indicates ALONE pattern, so the 2 boards are not linked at this point. Any thoughts? TIA
Thanks,
Wang