Me and my group members have constructed a demonsration board with a CC8520, CC2591 and AIC3101 to simply function as a wireless stereo cable. The roblem is that even though we can program each CC8520, and can see the pairing LED flash, we cant get them to pair, in fixed network ID mode or with the button, the pairing LED just stays in standby mode.
As the chip seems to be functional we can only conclude one of 3 things:
1. Either we're doing something stupid with the configurator,
2. There is an error with the way we're using the range extender
3. Or the crystal oscillator we are using isnt accurate enough for RF - it should be though, its rated at 50ppm.
I was hoping someone with experience could tell us if there is an obvious error in our schematic.