• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Low Power RF & Wireless Connectivity » Low Power RF PurePath Wireless Audio Forum » All Tags » AUDIO
Share
Low Power RF & Wireless Connectivity
  • Forums
  • Announcements
  • Files
  • E2E Wiki

Browse by Tags

Low Power RF & Wireless Connectivity

Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
AUDIO
  • 8520 8530
  • AIC3204
  • audio codec
  • audio transceiver transmitter receiver handset radio project
  • Audio Translation
  • c8520
  • C8520 wireless audio near-field interference
  • cc2590 cc8520 hgm gain
  • CC8520
  • cc8520 AIC3101 AIC3101EVM
  • CC8530
  • cc8531
  • CC85xxDK
  • GI02
  • Headphone
  • Headset
  • inductance
  • Microcontroller
  • Pure Path
  • Purepath
  • Purepath wireless audio
  • PurePath Wireless Configurator
  • USB driver
  • Wireless
  • Wireless audio
Related Posts
  • Forum Post: packaging the cc8531

    Hugo Sapin Hugo Sapin
    Hello, I would like to know if someone have any recommandations about the packaging of the CC8531 ? I am about to run some tests with it and would like to movve it easily and put it in a plastic case. Is it going to block the audio signal i am sending ? Thanks for your answer Hugo
    on Mar 19, 2012
  • Forum Post: Transmission problem with CC8531DK Headset

    Hugo Sapin Hugo Sapin
    Hello, I am trying to use the CC8531DK HEADSET to transmit audio from my laptop using a master in the "USB stereo soundcard" configuration to a slave card in the "generic stereo output" configuration that i am listening with headphones. So far everything works even if sometimes...
    on Mar 19, 2012
  • Forum Post: PurePath CC8530 and TLV320AIC3204 Design Help

    Juan Munoz Juan Munoz
    Hi, I have a few questions regarding the PurePath Development Kit and the CC85xx chip. 1. I would like to use the CC85xx chip for wireless audio but I would like to control it with and MCU. I bought the PurePath headset development kit and saw that the CC85xx chip is programmed via your CC...
    on Mar 14, 2012
  • Forum Post: multiple slave addressing in TLV320AIV26 sample code.

    pradeesh thomas pradeesh thomas
    Hi, i made a circuit using TLV320AIC26 and CC1110 (reference from AN-082), it works fine with two way and one way sample code (swra295a). Now i want to know how we can adress multiple slave in this. i don't want broadcast, i need communication between Master - slave1, master - slave2, slave1...
    on May 29, 2012
  • Forum Post: USB and I2S master without reprogramming

    Pavel Ruzicka Pavel Ruzicka
    Hello, I want to create HiFi stereo wireless connection to my DAC. On slave I simply connect I2S output from CC85XX to my 2x PCM1704 based DAC with I2S data format. On the Master I want USB input and also S/PDIF input (via DIR9001 to I2S). I understand that I can reprogram CC85X1 for USB input OR for...
    on Jul 7, 2012
  • Forum Post: CC85xx external clock

    Hugo Sapin Hugo Sapin
    Hello, I am using the cc8531DK Headset to transmit data. But as i would like to transmit 4 audio channels in PCM (16 or 24), i have to use 2 master cards and 2 slave cards. I would like to synchronize the 2 masters so the signals i receive on the slaves are synchronized too. My problem is that i...
    on Jul 12, 2012
  • Forum Post: Wireless audio to a large number of devices?

    Geoff Luck Geoff Luck
    Hi, I have a question about simultaneous and synchronised wireless audio transmission to multiple devices. I'm involved in a research project examining the effect of physical separation on music ensemble interaction and timing. Basically, I'm investigating how physically separating musicians...
    on Sep 1, 2012
  • Forum Post: PurePath CC85xx + CC259x EN300 328 v1.8.1 compatibility

    Nicolas Boulot Nicolas Boulot
    Hello, A new EN300 328 version will soon be published : v1.8.1. With more than 10 dBm (using CC259x range extension), LBT is required before transmit with at last 15 Frequency hopping. Does the actual firmware is compatible with this new version ? Thanks. Regards, Nicol
    on Sep 13, 2012
  • Forum Post: RE: stand alone, audio device

    Rahul Mittal Rahul Mittal
    Hi GENIUS (KJETIL) Thanks for your replies and time. I think we need to re design and fabricate the solution as per present requirements. Like mentioned above we can have wireless transmission through RF, but we need it through GPRS, through a GSM modem. Now Having said that we have modem. WE...
    on Sep 18, 2012
  • Forum Post: stand alone, audio device

    Rahul Mittal Rahul Mittal
    HI Its always great landing to your webportal, looking for something that suits my requirement. Please help me for one of such I want to develop a product ,which work as follows Call/connect to the specified web link.( may be through a GSM/Local Wifi connection) Receive the data from that link/server...
    on Sep 2, 2012
  • Forum Post: SPI link from master to slave

    Thomas Holm Thomas Holm
    Hi Im doing a wireless speaker system with a master unit and a slave unit. Transferring audio data from master to slave with CC85xx. In both speakers I'm using the PCM4104. I want to link the SPI instructions from to master to the slave so both PCM4104 receive the same instructions. How do I set...
    on Nov 2, 2012
  • Forum Post: CC8530 Audio Reset PP output performance

    Geovid Kali Geovid Kali
    Hi, In the PurPath Configurator there is a signal GIO2/Audio Reset in the IO section. I believe this is an output from the CC8530. How does this output perform? Does it hold reset when the radio is not passing audio or not connected? Is there a place that describes the behavior of the pin in the configurator...
    on Nov 19, 2012
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use