Hi experts,
How to enter and exit PW2?
when in PW2, is the 8-KB SRAM content is persistent, or it's gone?
Thanks,
Jerry
Hi Jerry,
When you use the OSAL framework that is associated with the BLE stack, PM2 is automatically entered when there are no tasks active (assuming power management is turned on).
SRAM contents are retained in all power modes. The only thing that will erase SRAM is if power is removed from the device.
Best regards,
Karl
Hello
I want to use the sleep timer to my dongle ,i want that my dongle wakeup all 5ms and look if there is the device wich wantto conncete whith him if not it return to sleep state ,i want to supprimed the pressed swicth to connecte
ca you help me please
Hi Abderrahmane,
the dongle is always powered, I think it cannot sleep.
Also, I suggest you to put your source code and then ask some questions, you will obtain much better results and answers than if you expect people to write code from scratch.
Good luck.
Please click the Verify Answer button on a post if it answers your question! :)
good morning
thank you for your reponse
when i press fastly in the remot control these last plant ,i verified my frame dongle, i recieved the press and release then i will compte the time between the release and the press to distinct if it is the repeat or not but my the problem of plant i can not deteminete where
these is the frame
thank you
Hi Ab,
you should open a new single thread for this, since with the old thread title, nobody is going to check your new problem ;)
Please, also try to present your info and doubts as clearly as possible. For example, I was unable to understand your last question due to the lack of info.
Bye! :) And good luck.
Edit: I've seen you have posted your question in ALL the other threads.
This is not correct at all. Please delete your posts since they are completely polluting the whole forum.
I am using cc2540 BLE for remote control ,when i press fastly in thekeu of remot control these last plant ,i verified my frame dongle, i recieved the press and release then i will compte the time between the release and the press to distinct if it is the repeat or not butwwhat caused the plant of the remote ,these is the frame of my dongle
ok
Sorry I'm new in to the site and I don't know how it works! I
i try to supprime all the message but i don't know where!! can you help me please
Login, check on the thread list the subjects where you are the latest poster. Enter in each one of them and press the red cross below your comments, when available. And do not repeat such a thing, since it provokes a lot of confusion :)
Bye.
Hi
I am using cc2540 BLE for the control remot i want to help me if you can!,i have the problem in the remot when i press in the key of the remot with small speed between the press, the dongle detect the press and release key very well but when i presse quiqly (time between the press is small) the dongle don't detect the release and stat as repeat stat so i don't know where is the problem ,i think these problem caused by accumulation of message event in the dongle.is the speed between the press key limited in cc2450