Hi,
Can someone help me with the setup for a (automatic) connection between the Keyfob and Dongle without using BTool?
I'm using now: Keyfob example for the KeyFob and SimpleBLECentral example for the USB Dongle.
Any help on which settings I should set, or maybe a simple code or example will be appriciated.
I've read alomost every document on this, but I can't find the solution....
Willem.
... has no one any idea? Any help will be appriciated!
Is there really nobody who can help me with this?
Hi Willem,
you have plenty of examples in the Linux section at the top of the post :)
They are easily modifiable to fit what you are asking for.
Good luck!
Please click the Verify Answer button on a post if it answers your question! :)