• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Low Power RF & Wireless Connectivity » Low Power RF Bluetooth® Low Energy & ANT Forum » which pins should be used as UART in DTM?
Share
Low Power RF & Wireless Connectivity
  • Forums
  • Announcements
  • Files
  • E2E Wiki
Options
  • Subscribe via RSS

which pins should be used as UART in DTM?

which pins should be used as UART in DTM?

This question is not answered
Lei Xia99765
Posted by Lei Xia99765
on Mar 13 2012 00:38 AM
Prodigy35 points

details about BLE Stack 1.2 Released:

http://e2e.ti.com/support/low_power_rf/f/538/t/166931.aspx

The article referred:

- Support for "Production Test Mode" has been added, allowing a BLE application in a "single-chip" configuration to temporarily expose the HCI over the UART interface when triggered externally to do so (e.g. hold a GPIO pin low during power up). This allows the device to be connected to a Bluetooth tester in order to run direct test mode (DTM) commands on a production line using the final release firmware, while leaving the UART GPIO pins available for the application to use at all other times

1) Which pins(CC2541) shoulod be used as UART in DTM? Or which pins you will recommend to be used as UART in DTM?

2) "(e.g. hold a GPIO pin low during power up). " Which GPIO pin should be used?

Thanks.

CC2541
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Peng Jeff
    Posted by Peng Jeff
    on Mar 29 2012 03:58 AM
    Prodigy230 points

    Yes!  Same problem here!

    The README.txt of BLE Stack 1.2 mentions:

    - Support for "Production Test Mode" has been added, allowing a BLE application
      in a "single-chip" configuration to temporarily expose the HCI over the UART
      interface when triggered externally to do so (e.g. hold a GPIO pin low during
      power up). This allows the device to be connected to a Bluetooth tester in
      order to run direct test mode (DTM) commands on a production line using the
      final release firmware, while leaving the UART GPIO pins available for the
      application to use at all other times

    We are going to do the Qualification Test to our product at Bluetooth Qualification Test Facilities (BQTF).

    Does this new feature help?  How do we use it exactly?

    Best regards,

    Jeff

    BLE stack 1.2 PTM Production Test Mode direct test mode DTM
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Joakim Lindh
    Posted by Joakim Lindh
    on Mar 29 2012 06:19 AM
    Genius13370 points

    Hi,

    Assuming that you are familiar with our BLE stack, the SW needs modification at applications layer to support PTM testing even though PTM is built in for BLEv1.2. We don’t have PTM documented yet, but the code below can be used in (for example) simpleBLEPeripheral.c  to show of how the application checks whether an MT8852B tester is connected during startup. It works by checking whether GPIO P0.4 is held low, and if it is then the application will enable PTM. Anritsu has implemented software in the MT8852B that will hold that line low to signal to the CC2540 (Pin P0.4 is exposed on the DB-9 header connecting to the MT8852B). The other pins are the normal pins used for the HCI interface when using a network processor build.
    Essentially, all PTM does is allows you to expose the physical UART HCI interface in a single-chip build, only when triggered by some action during initialization. In the case of the sample code, the action is pin P0.4 being held down by the MT8852B. On the production line when the MT8852B is connected, the device will initialize into PTM. Under all other circumstances (such as when the end-user powers up the device as a final product), the GPIO will not be held low, so the device will initialize as normal. The HCI interface is not exposed to the physical UART interface, and those GPIO pins can be used by the application for anything. This allows one single software build to be used for both production testing as well as the final application.
    Add following to constant declaration
    //-----------------------------------------------------------
    // TI BLE CC254x Production Test Mode
    #define PTM                   4
    #define RDY                   5
    #define PDUP0                 5
    #define P0ICON                0
    #define TESTER_CONNECTED()    (P0_4==0)?TRUE:FALSE
    //-----------------------------------------------------------
    Define and use the following function to setup the interface;
    //-----------------------------------------------------------
    /*******************************************************************************
     * @fn          llSetupPTMTestPort
     * @brief       This routine is application sample code that shows how to setup
     *              two GPIOs used as the RS232 flow control pins for the Production
     *              Test Mode header interface. This interface assumes UART0, Alt 1.
     *              The RTS is mapped as a pulled-up input and is used to determine
     *              if a Tester connector is attached to the PTM header. If RTS is
     *              asserted (low), then the connector is attached and PTM can be
     *              enabled; otherwise the application can boot normally. 
     *
     *              Note: The DUT's RTS is de-asserted. If PTM is enabled, then when
     *                    this pin is configured as part of the UART flow control,
     *                    its value will be asserted, which indicates to the Tester
     *                    that the DUT is ready.
     */
    void llSetupPTMTestPort( void )
    {
      // ready UART0, Alternative 1 for the application to monitor
      P0SEL &= (~BV(PTM) & ~BV(RDY)); // GPIO
      P0DIR &= ~BV(PTM);              // input; this is Tester's RTS
      P0DIR |=  BV(RDY);              // output; this is Tester's CTS
      P0    |=  BV(RDY);              // de-assert Tester's CTS
      P0INP &= ~BV(PTM);              // pull-up/pull-down depending on P2INP
      P2INP &= ~BV(PDUP0);            // pull-up
      return;
    }  
    //-----------------------------------------------------------
    Add the following to the Init function (Ex. SimpleBLEPeripheral_Init) and put the previous content in the else case
    //-----------------------------------------------------------
      llSetupPTMTestPort();
      
      // check if Tester's RTS is asserted
      if ( TESTER_CONNECTED() )
      {
        // it is, so enable PTM
        // Note: It is assumed when the Tester is finished, the connector will be
        //       removed from the DUT's header, and the DUT will be reset/power cycled.
        
        osal_pwrmgr_device( PWRMGR_ALWAYS_ON );
        
        HCI_EXT_EnablePTMCmd();
      }
      else
      {
        //moved here due to PTM test
        osal_pwrmgr_device( PWRMGR_BATTERY ); 
        //Copy and Past the original init content here
      }
    I hope this helped you to understand PTM further.
    Br
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • J Chan
    Posted by J Chan
    on Apr 05 2012 05:04 AM
    Prodigy90 points

    Hello Nick,

     

    Already tried incorporating the mentioned changes and did see the GPIO P0.4 is held low by MT8852B but still failed to perform test.

    Which EUT control shall be selected from the Anritsu tester application?  the baudrate to use?

     

    thank you

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Peng Jeff
    Posted by Peng Jeff
    on Apr 06 2012 23:10 PM
    Prodigy230 points

    Hello Nick,

    Thanks for the great detail!

    Our Bluetooth Qualification Test Facilities uses the BITE T1111 RF Test System.
    I need to confirm how the pins connect to RS232 when I use your PTM code.

    CC2540  <<<=======>>>  Tester

    UART0, Alt 1.                          RS232C
    ----------------------------------------
    P0.2:RX    <<<==========  TX
    P0.3:TX    ==========>>>  RX
    P0.4:CT    <<<==========  RTS
    P0.5:RT    ==========>>>  CTS
    ----------------------------------------

    Are these connections correct?  
    Do I have to connect all these four pins?
    Are there other pins I should connect to RS232?

    And, what baudrate should I use?

    Thanks for your help!

    Jeff

    CC2540 Serial interface BLE cc2540 BLE stack 1.2 PTM DTM RS232
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Per H
    Posted by Per H
    on Apr 16 2012 02:56 AM
    Expert6750 points

    Hi Jeff,

    I have not run the BITE system myself but I do know some of our customers does so it should work fine!

    Connect all 4 pins as you have shown. The set-up opf the instrument should be:

    Baudrate -> 57600

    Databits -> 8

    Stop bits -> 1

    Parity -> None

    Protocol -> None

    Let me know if it works!

     

    -Per

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Joakim Lindh
    Posted by Joakim Lindh
    on Apr 17 2012 07:40 AM
    Genius13370 points

    Hi,

    I have updated some information regarding DTM/PTM on our wiki: 

    http://processors.wiki.ti.com/index.php/PTM

    Have a look there and see if you've missed anything.

    Br

    http://processors.wiki.ti.com/index.php/PTM

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • J Chan
    Posted by J Chan
    on Apr 23 2012 02:43 AM
    Prodigy90 points

    Hello Nick,

    Still not able to make it work...
    From the wiki you mentioned that the DUT's RTS will be asserted, which indicates to the Tester that the DUT is ready.  But P05 remains high even after EnablePTM.
     
    I also tried using BTool to issue the HCIExt_EnablePTM to a cc2541 with CC2541_SmartRF_HostTestRelease_All.hex firmware.  
    I got an unknown hci command status.


    12] : <Tx> - 03:03:41.047
    -Type  : 0x01 (Command)
    -Opcode  : 0xFC0E (HCIExt_EnablePTM)
    -Data Length : 0x00 (0) byte(s)
    Dump(Tx):
    01 0E FC 00

    ------------------------------------------------------------------------------------------------------------------------
    [13] : <Rx> - 03:03:41.109
    -Type  : 0x04 (Event)
    -EventCode : 0x0E (HCI_CommandCompleteEvent)
    -Data Length : 0x04 (4) bytes(s)
     Packets  : 0x01 (1)
     Opcode  : 0xFC0E (HCIExt_EnablePTM)
     Status  : 0x01 (Unknown HCI Command)
    Dump(Rx):
    04 0E 04 01 0E FC 01

    any idea what i've done wrong?

    tnx, J

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Joakim Lindh
    Posted by Joakim Lindh
    on Apr 25 2012 02:27 AM
    Genius13370 points

    Hi J,

    Did you follow the code examples in the "How to Use PTM from an Application Point of View" section? Have you connected the Anritsu correct?

    As for the HCIExt_EnablePTM it says in the TI BLE Vendor Specific HCI Guide: 

    This command is used to enable Production Test Mode (PTM). This mode is used by the customer during assembly of their product to allow limited access to the BLE Controller for testing and configuration. This command is only available when the BLE Controller is built without external access to the Controller (i.e. when no transport interface such as RS232 is permitted). This mode will remain enabled until the device is reset. Please see the related application note for additional details. Note: This command is only allowed as a direct function call, and is only intended to be used by an embedded application.
    So you cant use the HCIExt_EnablePTM command over a serial connection. You could use HCI_LE_Transmitter_Test instead, as described on the wiki.
    Br 
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • J Chan
    Posted by J Chan
    on Apr 25 2012 06:37 AM
    Prodigy90 points

    hello nick,

    yes, did follow the sample code snippet. and did verifiy the function was called by setting a break point.

    i was able to run the anritsu tester with the cc2540 module running the CC2540_SmartRF_HostTestRelease_All.hex.  EUT control set to rs232 with 57600 baudrate.

    but for this PTM, regardless whether i set the EUT control to RS232 or bi-wire, it doesnt work.  how do i know whether cc2540 is really running in test mode?

     

    thanks

    regards, J

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Joakim Lindh
    Posted by Joakim Lindh
    on May 02 2012 04:01 AM
    Genius13370 points

    J, 

    Make sure that you do have HCI_DISABLE_UART defined. To check if the HCI_EXT_EnablePTMCmd was successful, make sure that the return value is 0x00. 

    Br

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • J Chan
    Posted by J Chan
    on May 16 2012 05:59 AM
    Prodigy90 points

    Hello Nick,

     

    there is no HCI_DISABLE_UART in the list of preprocessor defined symbols and i did get a 0x00 from calling HCI_EXT_EnablePTMCmd.

     

    Regards,

    J

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Chi-wen Wang
    Posted by Chi-wen Wang
    on May 16 2012 16:14 PM
    Intellectual690 points

    Hi Nick,

      I have two questions on your description.

      1. Does HCI_EXT_EnablePTMCmd only work with UART_0?  We just need to understand if UART_1 can be used due to some constraints with our pin assignments.

      2. For UART_0, can HCI_EXT_EnablePTMCmd only work with alternative 2?  That is, can we use (P1.5, P1.4, P1.3, P1.2) as UART_0 for DTM/PTM?

    CC254X DTM PTM
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Joakim Lindh
    Posted by Joakim Lindh
    on May 21 2012 02:23 AM
    Genius13370 points

    Hi Chi-wen,

    I have updated the wiki (http://processors.wiki.ti.com/index.php/PTMhttp://processors.wiki.ti.com/index.php/PTM) with further information on this matter. Please have a second look. The UART config is fixed in the library file so you would have to use UART 0 for DTM/PTM.

    Best Regards

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Chi-wen Wang
    Posted by Chi-wen Wang
    on May 21 2012 09:38 AM
    Intellectual690 points

    Hi Nick,

      Thanks.

      Could you also answer my 2nd question in the previous post?

       2. For UART_0, can HCI_EXT_EnablePTMCmd only work with alternative 2?  That is, can we use (P1.5, P1.4, P1.3, P1.2) as UART_0 for DTM/PTM?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • J Chan
    Posted by J Chan
    on May 24 2012 04:40 AM
    Prodigy90 points

     

    Hello Nick,

     

    so following the updated wiki, I have made sure that the HCI_DISABLE_UART, HAL_UART, and HAL_DMA=TRUE are defined in the project options.

    and i noticed that there is this "f0 50 10 d0" data coming from cc254x on power up from the uart port.  may i know what is this 4 byte data conveying?

     

     

    thank you

    j

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
12
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use