How many devices can be connected (wirelessly) to the CC2570 and how many to the CC2571? For example let's say I am wearing both a heart monitor strap and an accelerometer. My understanding of the CC2570/71 datasheet (p.11) is that the heart monitor and accelerometers would each be Client/Masters and the CC2570 or CC2571 would be the Host/Slave. My follow-on question is this: if both can support communications with multiple devices, what does the CC2571 have that the CC2570 doesn't? Multiple Nodes or Endpoints?
Hello,
The difference between the CC2570 and the CC2571 is that the CC2570 supports 1 ANT channel, while the CC2571 supports 8. Therefore, you could connect 1 wireless device to a CC2570, and 8 to a CC2571.
Cheers,
Kassandra