All,
I'm using IAR 8.11.1 and upgraded to the 1.2.1 release. I'm able to compile all the example Apps but cannot download to target with debugger. Clicking the download and debug button updates the build tree but stops after that. I saw an error about IdataStack is at 100% (192 of 192), threshold set to 90% etc. I couldnt get that error again.
I can go back to the 1.1a release and I can download to target.
Is there a flag to enable a debug build perhaps ? Any help will be great.
Cheers
J
Rebuilding entire target for every debug download seems to fix the problem. A bit painful but get me going.