Hi there, I am bringing up our new radio board, which includes the CC2541 128. I have the debugger wired into a header on the board and can download my program and step through it, so things seem okay at that point and the BLE stack claims it is advertising. However, I am not seeing any advertisements from my iOS app. The BLE app was initially developed on the CC2540 and worked fine. Apparently there are differences in the BLE implementations between the 2540 and 2541 so I believe i have updated the BLE library correctly (to CC2541_BLE_peri.lib), added a CC2541 flag to the buildConfig.cfg preprocessor file , and updated the debugger ddf for the 2541. Is there anything else I need to do? Looking at the other 2541 files, I am not seeing any differences. I do notice the linker file is using a 2540 file for other example projects such as the key fob app. Is this okay? Anything else to change? And if not, is there a way for me to get a better idea of the radio transmit status in the case that this a board problem?
thanks!
-Tyler