• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Low Power RF & Wireless Connectivity » Low Power RF Bluetooth® Low Energy & ANT Forum » All Tags » 2540
Share
Low Power RF & Wireless Connectivity
  • Forums
  • Announcements
  • Files
  • E2E Wiki

Browse by Tags

Low Power RF & Wireless Connectivity

Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
2540
  • #CC2540 #OLP425 #I/O
  • 2540 GATTServApp_RegisterService const
  • 2540 IAR
  • 2540 profile
  • 2540 UART
  • 2541
  • ADC
  • Advertising
  • Android OS
  • ANT
  • ANT+
  • beginner programming CC2540
  • BLE
  • BLE CC2540
  • BLE cc2540
  • BLE stack
  • BLE V1.1
  • Bluetooth
  • Bluetooth Low Energy
  • Bluetooth Low Power
  • BTool
  • C2540
  • CC 2540
  • CC2540
  • cc2540 & Bluetooth Low energy
Related Posts
  • Forum Post: CC2540 ID1257: - Flash erase failed

    Dzuong Nguyen Dzuong Nguyen
    I'm having trouble erasing the CC2540 flash. I've just assembled my own CC2540 (256K) pcb using the keyfob layout as reference. I'm using a 3.3V regulator to power the CC2540 chip and also have the 32MHZ and 32KHZ crystals soldered on. The debug header pin assignments are almost exactly the...
    on Sep 7, 2012
  • Forum Post: CC2540 Communication between two Key Fobs

    Bobbie Gauna Bobbie Gauna
    Hi Team, I have two SDK for CC2540 and I am wondering if there's a way to set up one as a host and the other as a slave. If so, can I also use the test pins to read data off the master keyfob? My plan is to use the proximity code to communicate between different devices using the keyfob reference...
    on Dec 21, 2010
  • Forum Post: Re: cc2540 BLE 8051 Core

    mitaka mitaka
    I have a similar problem with getting an interrupt from Timer1. I have the mini dev kit. Timer1 is in modulo mode and T1OVFIM = 1; // Enable overflow interrupt T1IE = 1; // Enable Timer 1 interrupts by setting [IEN1.T1IE=1] EA = 1; // Enable global interrupt by setting the [IEN0.EA=1] the...
    on Jan 7, 2011
  • Forum Post: BLE range for CC2540 keyfob in the indoor(including walls)

    Younes Rashidi Younes Rashidi
    Hi, I'm going to use CC2540 "Keyfob" in the office building (two floor and each floor is 1500m2) and I want to know: 1- CC2540 keyfob indoor range 2- Does BLE stack support repeater operation? I mean, if I use a CC2540 Keyfob as a repeater (to achieve longer range), BLE stack support...
    on Jan 6, 2011
  • Forum Post: Re: Can CC2540 USB master dongle work with more than one CC2540 Keyfob slaves?

    Younes Rashidi Younes Rashidi
    Hi, Karl, I've already done a project with Zigbee in which one CC2531 USB Dongle was coordinator and ten CC2530EM were End Device and recently my client asked me to do this job with BLE (one CC2540 USB dongle and ten CC2540 keyfob). So you mentioned CC2540 cannot support multiple simultaneous...
    on Jan 12, 2011
  • Forum Post: Re: Can CC2540 USB master dongle work with more than one CC2540 Keyfob slaves?

    Younes Rashidi Younes Rashidi
    Hi Karl, Thanks for your suggestion. one more question please, can two CC2540 USB dongle communicate with each other? Thanks,
    on Jan 12, 2011
  • Forum Post: Re: Can CC2540 USB master dongle work with more than one CC2540 Keyfob slaves?

    Younes Rashidi Younes Rashidi
    Hi Karl, Thanks, that's great! Can the CC2540 USB dongle work in the procedure in which it repeatedly be configure as a master and read data from CC2540 keyfob and then be configure as slave and send data to another CC2540 USB dongle (with master cofiguration)? best regards,
    on Jan 12, 2011
  • Forum Post: Compatibility of BLE stack with other tasks

    Vasco Tesi Vasco Tesi
    Hello, my question is around the compatibility of BLE stack with other tasks that could be implemented on CC2540 SoC. Is it possible to use Timer 1 for the generation of PWM signals , or set a repeated ADC conversion through DMA, and at the same time maintain a BLE connection , without problems...
    on Jan 31, 2011
  • Forum Post: Problem connecting the dongle to a PC

    Gijs de Graaf Gijs de Graaf
    Hello, I'm a student and just started my graduation assignment. For this I'm trying to use the CC2540 Mini Development kit. Now I've encountered a problem with getting the kit to work, when I connect the dongle to my PC it doesn't get recognized. The dongle does get power...
    on Feb 3, 2011
  • Forum Post: Slave BDA address on CC2540 Mini Development Kit keyfob

    John Smith61414 John Smith61414
    Hi, How can I change the Slave BDA address on the keyfob for the CC2540 Mini Development Kit? I would like to have a unique address so that several keyfod's can be used simultanious. Thanks, John
    on Nov 24, 2010
  • Forum Post: Pre-loaded firmware source code

    Enid Juan Enid Juan
    We bought cc2540 minidk module and downloaded the developing libraries. We also verified the pre-loaded firmware with BTools. But when we tried to write some modifications of SimpleBLEPeripheral source code, the module came into no-response and the document gave us very little help. Could...
    on Mar 11, 2011
  • Forum Post: Software implementation of I2C on CC2540

    Epic Vancouver Epic Vancouver
    we are using the CC2540F128 on our design. We want to use P1_6 and P1_7 to implement a bit-banged I2C interface so we can talk to a temperature sensor, such as the TMP102. Does TI have any example code for a software implementation of I2C on a CC2540F128 chip? Please advise asap ...
    on Apr 8, 2011
  • Forum Post: CC2540 FOB status 0x11

    Hansen Dsouza Hansen Dsouza
    Hi, I set a secondary address on the CC2540 it was previously reading primary and secondary as fffffff. How do i read the primary address?in the flash programmer i just get the secondary address. After setting the secondary address I try to establish a connection to it but i get a message immediately...
    on Feb 25, 2011
  • Forum Post: HostTestRelease slave example / setup

    Geoffrey Kruse Geoffrey Kruse
    I'm attempting to use the HostTestRelease project in the USB slave configuration. I'm able to go through the steps to make the device discoverable, however I can not discover it using BTool. All of the responses from the CC2540 indicate that my HCI commands are successful. I must be missing a...
    on Feb 9, 2011
  • Forum Post: Question about CC2540 RF registers

    Jianfeng Lv Jianfeng Lv
    Hi sir, I plan to use CC2540 in my project. However, unlike CC2530, I didn't find any information about registers that control RF part of CC2540 in the user's guide (swru191b), only status registers are available. Since the BLE stack is not open source, it means that both hardware and software...
    on Aug 19, 2011
  • Forum Post: How to support streaming Data with BLE profiles?

    Nick Close Nick Close
    I am working on a new project that uses the CC2540. I will need to support some of the standard BLE profiles but I also need to be able to stream some data. I am assuming that I will need to create a custom profile to do this, is this correct and if so how do I go about this (i.e. Do I need to generate...
    on Sep 5, 2011
  • Forum Post: Accurate timing using OSAL on CC2540

    Nick Close Nick Close
    For a project that uses the CC2540, I need to perform ADC conversions periodically (every 4ms). It doesn't matter if there is some jitter in the time between conversions as long as it averages out to 4ms (+/- 10us). I could use one of the available timers to generate a periodic interrupt to achieve...
    on Oct 6, 2011
  • Forum Post: (cc2540) about advertisement data of GAP

    choi chuljin choi chuljin
    Hello, sir. i was TEST period data transfer use sniffer packet program and provide example. project SimpleBLEperipheral and HostTestApp download to each devices, and watching the sniffer program. after than, i some change the program code. advertisement data array "static uint8 advertData...
    on Oct 14, 2011
  • Forum Post: IEEE address in the information page of the CC2540 not unique?

    Brandon Kinman Brandon Kinman
    Hello, It appears that the reportedly unique (according to the CC2540 User Guide) 48-bit IEEE address stored in the information page beginning at address 0x780E of the CC2540 is not unique, but is in fact {0xCO,0xFF,0xEE,0xCO,0xFF,0xEE}. Is this correct? If so, how would you recommend going about...
    on Aug 10, 2011
  • Forum Post: CC2540 USB Dongle - Mac OS X Lion

    Anton Kiland Anton Kiland
    I am having issues connecting my CC2540EMK-USB dongles to Mac OS X 10.7 Lion. They are correctly recognized as CDC-devices and all the USB information shows up in USB Prober, although dmesg reports the following: AppleUSBCDC: start - initDevice failed Nothing shows up under /dev/cu.* or ...
    on Oct 22, 2011
  • Forum Post: GAP_LINK_TERMINATED because of supervisor timeout

    Gergo Zsiak Gergo Zsiak
    Hi All, We faced with problem, namely the BLE link used to terminate with the reason 0x08 "Supervisor Timeout". The soluiton was the setting of DEFAULT_UPDATE_CONN_TIMEOUT to a larger value. It works now correctly, but we couldn't figure out the reason. The server sends notifications...
    on Oct 27, 2011
  • Forum Post: CC2540 UART and Low Power Mode

    Nick Close Nick Close
    I am currently working on a project that includes a CC2540 and an MSP430 in the design. The two devices are connected together via a UART. The MSP430 will be sending data to the CC2540 over the UART interface once a second and the CC2540 will use this data to transmit over BLE when connected to a...
    on Nov 18, 2011
  • Forum Post: Help with Windows 7 driver for CC2540 USB Dongle

    Michael Hoyt Michael Hoyt
    I'm trying to get through chapter 3 of the mini developers kit user guide. I can't get past the USB Dongle driver association step. Windows is complaining about an unknown USB device. When I try to install the driver from : C:\Program Files (x86)\Texas Instruments\SmartRF Tools\Drivers\Cebal...
    on Nov 24, 2011
  • Forum Post: Primary IEEE address of CC2540

    Leo Choi Leo Choi
    I have two CC2540EM. Both of them are having the same IEEE Adreess (0xC0FFEEC0FFEE). Is all cc2540 has the same address? how can i distinguish two modules with the BTLE stack? The Rev number of the modules is Rev .1.5.1.1
    on Dec 5, 2011
  • Forum Post: USB Drivers (virtual com port)?

    Stan 59800 Stan 59800
    Are there available any cc2540 (cc2531 etc) USB drivers (virtual com port) for other OS beside Windows x32/x64? Does TI intend to release soon and drivers for any of the other popular OS like Linux,Win CE, iOS, Android? If not – what resources are available to help me do it myself? Is the...
    on Jan 7, 2011
12345»
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use