• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Low Power RF & Wireless Connectivity » Low Power RF Bluetooth® Low Energy & ANT Forum » All Tags » CC2540
Share
Low Power RF & Wireless Connectivity
  • Forums
  • Announcements
  • Files
  • E2E Wiki

Browse by Tags

Low Power RF & Wireless Connectivity

Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
CC2540
  • #CC2540 #OLP425 #I/O
  • 1.2.1
  • 2540
  • 2540 GATTServApp_RegisterService const
  • 2540 IAR
  • 2540 profile
  • 2540 UART
  • 2541
  • 8051
  • ADC
  • Advertising
  • Android OS
  • ANT
  • ANT+
  • beginner programming CC2540
  • BLE
  • BLE CC2540
  • BLE bluetooth
  • BLE cc2540
  • BLE stack
  • BLE stack 1.2
  • BLE V1.1
  • Bluetooth
  • Bluetooth Low Energy
  • Bluetooth Low Power
Related Posts
  • Forum Post: HostTestApp on CC2540EB -- invalid Profile Role??

    Miles Guidon Miles Guidon
    I have The CC2540EB configuration of HostTestApp running on the CC2540 key fob that comes with the TI mini dev kit. I have a PIC24 MCU providing UART HCI to the key fob, and I am trying to send the three GAP commands to make the device discoverable by the USB dongle, using BTool during a "Scan"...
    on Jun 9, 2012
  • Forum Post: Re: CC2540 - Temperature Sensor

    Kjetil Kjetil
    Hi. If you can't use the internal one then Texas Instruments has a whole range of temperature sensors: http://focus.ti.com/analog/docs/sensorshome.tsp?familyId=353&contentType=4 I'm sure you can find one suitable for your needs. Regards, Kjetil
    on Oct 14, 2010
  • Forum Post: Re: CC2540 External Reference Pin Out and Memory Block Size Question

    Karl T. Karl T.
    Mike, On question 1), yes, you should connect your external 2.2V reference to AIN7. Make sure to select AIN7 as a reference rather than the internal one (ADCON2). Karl
    on Oct 18, 2010
  • Forum Post: Re: can TI provide BTool source code for CC2540

    Kjetil Kjetil
    Hi Didier, I'm afraid the BTool is not available in source code. If this changes, we will post about it here in the forum section. Best regards, Kjetil
    on Oct 22, 2010
  • Forum Post: CC2540 Detailed Data Sheet

    Kay Reiche Kay Reiche
    The data sheet for the CC2430 has 212 pages, including a bit-by-bit description of all registers and much more. That one I found for the CC2540 has 33 pages and does include almost nothing. Is there any detailed data sheet available for the CC2540?
    on Oct 24, 2010
  • Forum Post: Re: CC2540 32.768 kHz Crystal Selection

    Karl T. Karl T.
    Hi Christopher, There are a lot of different crystals that can be used, with different size/cost trade-offs. In general, the most important things to look for is accuracy (a certain number of ppm over a certain temperature range), and load capacitance. As noted in the data sheet, we recommend the...
    on Nov 11, 2010
  • Forum Post: Software crashes

    Cameron Patterson Cameron Patterson
    In going through the CC2540 User's Guide, I'm finding that the BTool software crashes upon every successful data connection. I'm able to connect to the keyfob just fine, but when I read or write a characteristic value or something, it'll be successful but the software will immediately...
    on Nov 5, 2010
  • Forum Post: Defective CC Debugger?

    Cameron Patterson Cameron Patterson
    How can I know if my CC Debugger is defective? The SmartRFProgrammer software is installed as well as all necessary drivers, but it won't recognize the dongle or the keyfob from the CC2540 kit. Also, when I open SmartRFProgrammer, the software doesn't recognize the Debugger. Has anyone else encountered...
    on Nov 17, 2010
  • Forum Post: about CC2540 make files

    haiqun li haiqun li
    In BLE- CC2540 's Readme file,it says: The following software projects are included, all built using IAR Embedded Workbench v7.51A: But when I open the projects,the IAR prompt me like this: Thu Nov 25 16:35:03 2010: Warning: The device description file: C:\Program Files\IAR Systems\Embedded Workbench...
    on Nov 26, 2010
  • Forum Post: Re: Which current smart phones that can talk BLE?

    Michael Devine Michael Devine
    Thanks, Karl. I've since learned that some limited BLE support has made its way into the Android source tree (or at least into the BlueZ source tree). So, for now, I am going to bridge from an emulated Android phone to the CC2540 kit USB dongle. As soon as it's feasible, I might try to put...
    on Nov 30, 2010
  • Forum Post: CC2540 Communication between two Key Fobs

    Bobbie Gauna Bobbie Gauna
    Hi Team, I have two SDK for CC2540 and I am wondering if there's a way to set up one as a host and the other as a slave. If so, can I also use the test pins to read data off the master keyfob? My plan is to use the proximity code to communicate between different devices using the keyfob reference...
    on Dec 21, 2010
  • Forum Post: Re: 2540 Transmit Power

    Karl T. Karl T.
    Werner, I think the previous post was just an example. In practice, the CC2540 supports output power settings of -20, -6, 0 and +4 dBm. Best regards, Karl
    on Jan 3, 2011
  • Forum Post: Re: cc2540 BLE 8051 Core

    mitaka mitaka
    I have a similar problem with getting an interrupt from Timer1. I have the mini dev kit. Timer1 is in modulo mode and T1OVFIM = 1; // Enable overflow interrupt T1IE = 1; // Enable Timer 1 interrupts by setting [IEN1.T1IE=1] EA = 1; // Enable global interrupt by setting the [IEN0.EA=1] the...
    on Jan 7, 2011
  • Forum Post: BLE range for CC2540 keyfob in the indoor(including walls)

    Younes Rashidi Younes Rashidi
    Hi, I'm going to use CC2540 "Keyfob" in the office building (two floor and each floor is 1500m2) and I want to know: 1- CC2540 keyfob indoor range 2- Does BLE stack support repeater operation? I mean, if I use a CC2540 Keyfob as a repeater (to achieve longer range), BLE stack support...
    on Jan 6, 2011
  • Forum Post: Re: Can CC2540 USB master dongle work with more than one CC2540 Keyfob slaves?

    Younes Rashidi Younes Rashidi
    Hi Karl, Thanks for your suggestion. one more question please, can two CC2540 USB dongle communicate with each other? Thanks,
    on Jan 12, 2011
  • Forum Post: Re: Can CC2540 USB master dongle work with more than one CC2540 Keyfob slaves?

    Younes Rashidi Younes Rashidi
    Hi Karl, Thanks, that's great! Can the CC2540 USB dongle work in the procedure in which it repeatedly be configure as a master and read data from CC2540 keyfob and then be configure as slave and send data to another CC2540 USB dongle (with master cofiguration)? best regards,
    on Jan 12, 2011
  • Forum Post: Re: Doubts about BLE capacity.

    Frederico Frederico
    Hi, I´m thinking not open 8 connections at same time but open one connection per time and transmit the buffered data using CC2540 like example below: "I accept 100 ms delay, so I will divide this time for 8 sensors therefore each sensor has 12.5 ms of connection . The software will store...
    on Jan 17, 2011
  • Forum Post: Re: Doubts about BLE capacity.

    Frederico Frederico
    Hi Karl, At one connection what is the maximum data packet size? Frederico
    on Jan 17, 2011
  • Forum Post: Re: Question about GAP_DeviceDiscoveryRequest();

    Frederico Frederico
    Hello, 1 - I´m using ble_single_chip_master_pm_off.lib. 2 - I´m not finding at the code where the program process GAP_DeviceInitDone event, but the first command to discovery devices arrives 5 seconds after the system turns on. 3 - Yes, The parameter profileRole is set to GAP_PROFILE_PERIPHERAL...
    on Feb 4, 2011
  • Forum Post: This device cannot start. (Code 10)

    Robert Koch Robert Koch
    Hi, I downloaded the drivers that come with the BLE-Stack from TI but Windows XP is unable to start the device. "Add new hardware wizard" displays the following: Cannot Start this Hardware There was a problem installing this hardware: TI CC2540 Low-Power RF to USB CDC Serial Port ...
    on Jan 31, 2011
  • Forum Post: Re: Question about GAP_DeviceDiscoveryRequest();

    Frederico Frederico
    Hello, I corrected the startup gap parameters where the code is showed below: // Initialize the Profile Advertising and Connection Parameters gapRole_profileRole = GAP_PROFILE_CENTRAL; VOID osal_memset( gapRole_IRK, 0, KEYLEN ); VOID osal_memset( gapRole_SRK, 0, KEYLEN ); gapRole_signCounter...
    on Feb 4, 2011
  • Forum Post: Re: Question about GAP_DeviceDiscoveryRequest();

    Frederico Frederico
    Hello, The function device discovery request is working now. Thanks for your help! Frederico
    on Feb 4, 2011
  • Forum Post: LL master connectivity in current TI BLE stack

    Vasco Tesi Vasco Tesi
    Hi, a general question. In swru271 , TI BLE software development guide, at pag. 10 it's written "At this time, the CC2540 BLE Protocol Stack does not allow for a central device to have multiple simultaneous connections". This means that a piconet can not be set up at this moment ? ...
    on Feb 4, 2011
  • Forum Post: CC2540 test pin

    Marco55973 Marco55973
    Dear experts, I'm trying to add an analog sensor to the CC2540. In the Keyfob Reference Design I found that pin 1 and 3 correspond respectively to P0_6 and P0_7. I decided to use P0_6 as analog input and P0_7 to control the power feed of my sensor. I realized my Hal_sensor.c and .h files containing...
    on Jan 4, 2011
  • Forum Post: Re: BD_ADDR - How should I do to customize Bluetooth device address.

    Frederico Frederico
    Hello Greg, Yesterday I found the function "bStatus_t GAP_ConfigDeviceAddr (uint8 addrType, uint8 *pStaticAddr)" and I used it and now I´m able to modify the device address how I need. But, I have not been understanding well how to choose the better addrType parameter to my application...
    on Feb 8, 2011
12345»
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use