Hello,
I'm unable to communicate with pan1325 module. I supplied 3.3V to pin 11(CL1.5_LDO_IN) and 15(MLDO_IN), 1.8V to pin 22(VDD_IO), provide 32k clock to pin 8(SLOW_CLK_IN), drive pin 16(nSHUTD) high and pin 3(CTS) low. I'm using linux blueZ uart stack (hciattach /dev/ttyUSB0 any 115200 flow) and modified bt stack from LUFA library but I'm unable to get anything from the device. No activity on device's TX pin.
What can be possibly wrong?
Fero
Nothing attached. Looks like the file attach interface has changed :) Try zipping the file -- it wouldn't let me attach a plain .bts file
Fero,
Please see file attached in previous post in this thread.
Miguel
No change.
root@freescale /home$hciattach ttymxc3 texas 115200Initialization timed out.
No change. Same timed out error.
Don,
Could you check which bytes go through the UART interface?