Hi,
I am using MSP430F5438 evaluation kits, It's working fine with two boards with temperature application.
I want do the connection with my laptaub or iphone, What are the changes to be made to complete the connection and data sending?
While connecting to the laptaub the error messages are displayed on the LCD ACL disconnected and ERROR 0x15 flashing on the screen.
Regards
Amol
Amol,
The BT demo that you have will not connect with the iPhone. You need an apple authentication device in order to pair with the iPhone. To get it to pair with your PC, you need to change the name of the BT dongle on the laptop. Look at this thread here:
http://e2e.ti.com/support/low_power_rf/f/660/t/129753.aspx
To get it to pair with an iPhone, you would need to work with the BT stack vender to get the API's for talking to the MFI chip from Apple.
-Jason
---------------------------------------------------------------------------------------------------------Please click the Verify Answer button on this post if it answers your question.---------------------------------------------------------------------------------------------------------