Hello,
My name is Vassilis Klouvatos, I am new to Texas Instrument technology. I want to make a question. I am thinking building on a Sensor for capturing bio-signal from human body using ANT+ Wireless protocol. I want to integrateADS1191 with CC2570 in order to transmit the signal using ANT+ technology. Do I need an MCU in order to achieve the communication between these two modules? If I need MCU please can you provide me with information in order to find one?
Thanks in advance
Hi Vassilis,
Our CC2567 device features BT4.0+ANT. You can use the MSP430BT5190 as the host MCU (http://www.ti.com/product/msp430bt5190).
For evaluations use the PAN1323EMK(BT4.0+ANT,BT4.0+BLE), MSP-EXP4305438 Experimenter Board, and MSP-FET430UIF (each sold separately).
Our BT kits can be purchased from panasonic:
www.panasonic.com/ti
Regards,
ZH
------------------------------------------------------------------------------------------Please click the Verify Answer button on this post if it answers your question.
Please visit our CC256x Forum Guidelines and FAQs
Check out our CC256x Bluetooth Main Wiki page: http://processors.wiki.ti.com/index.php/CC256x
------------------------------------------------------------------------------------------