Hi,
We are using Bluetopia LE stack for our project.My user application consists of an audio playback at particular intervals.The problem now is whenever i tried to call my audio related file from the bluetopia stack its not working. I can just hear a beep sound through the speaker.Can anybody tell me the frequency settings required for playback audio with Bluetopia LE stack.When i load my user application alone without BLE stack it works fine, but when i try to add BLE stack and make a function call for audio from inside BLUetopia code itts not working, Why is this.What changes i have to make inorder to play my audio properly while in bluetopia stack