I am trying to run the cc256x msp430 Bluetopia Basic SSPDemo app on a TM4C123G Launchpad with CC256x QFN EM Board. In interfacing the CC256 to the to the TM4C123g I follow the info in HALCFG.h:
/* Function Port/Pin */
/* -------- -------- */
/* RX PC4 */
/* TX PC5 */
/* RTS PF0 */
/* CTS PF1 */
/* RESET PF2
The program compiles and loads but I get no output on teraterm when I reset the board as instructed.
I am wondering about the SLOW_CLK_IN line to the cc256x. Should I be providing this from some source on the TM4C123?
Thank you.