I have a project use MSP430F2370+TRF7970A.
But I don't know how to do read and write mifare classic cards.
Can help me?
Cann't to do that?
We are working on porting our Stellaris(Cortex M3) TRF7970A MIFARE code to MSP430F2370 currently. It should be ready to release in a few days. I have made a note and will let you know when this is ready.
Best Regards,
Eddie LaCost
---------------------------------------------------------------------------------------------------------Please click the Verify Answer button on this post if it answers your question.---------------------------------------------------------------------------------------------------------
Hello,
as this post:
Eddie LaCost We are working on porting our Stellaris(Cortex M3) TRF7970A MIFARE code to MSP430F2370 currently. It should be ready to release in a few days. I have made a note and will let you know when this is ready.
is already a few days old, I would like to ask if this ported code is already available and where to get it. I would also be interested in it.
Regards
Also am I
I'm waiting for this code long time..
Chris/Frank,
I sent you an e2e friend request with the information I need from you so that I can send this code.
I would also be interested.
Best regards,
Lukas Wilhelm
I am also interested . Is it already available ??
Manuel
Dear Eddie,
Where could I get the code?
Thanks!
Eddie,
Could you please send me a copy of the MIFARE code as well? Thank you!
Hello Eddie,
I acquired TRF7970A EVM and I'm making experiments with MSF430FR5739/MSP430F2370 and TRF7970A. Is it possible to have access to a working version of code to read and write MIFARE with MSP430F2370?
Best regards.
Hi Eddie,
could you please send me the source code of the project that will be used for read/write MIFARE Card?
Is this software available for MSP430 and Stellaris M3/M4 as well? Which is the part number that you use for the project? it will be useful in order to understand the right size of memory required by MCU for emulating the MIFARE protocol.
Thanks a lot,
BR,
Giordano
please request the M3 code from here ==> http://www.ti.com/tool/sw-dk-lm3s9b96-em2-trf7960-14443a&DCMP=STELLARIS®ARM®CORTEX+Other&HQS=Other+OT+sw-dk-em2-7960r
then i will know your email and are OK from a DE list check and can send you the updates for the MSP430 and the M3 for the TRF7970A.
Porting for the LM4F is in the queue ==> just waiting on the FW resource to open up.
BR-
Josh
Vitor and Giordano -
I just sent you guys an email for this like i said.