• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Low Power RF & Wireless Connectivity » RFID/NFC Forum » All Tags » 15693
Share
Low Power RF & Wireless Connectivity
  • Forums
  • Announcements
  • Files
  • E2E Wiki

Browse by Tags

Low Power RF & Wireless Connectivity

Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
15693
  • 14443a
  • 15693 collision DSFID
  • 7960
  • 7970 7960 rfid SPI
  • 7970 7960 rfid SPI TRF7970A EVM
  • 7970EVM
  • abd
  • amplifier
  • Antenna
  • C#
  • Fujitsu MB89R118
  • IRQ
  • ISO14443A
  • ISO14443A/B
  • ISO15693
  • ISO15693 RFID TRF7960
  • metal
  • MSP430
  • RFID
  • TRF7960
  • TRF7960 antenna
  • TRF7960EVM
  • TRF796x
  • TRF7970 EVM
  • trf7970 EVM
Related Posts
  • Forum Post: Increasing Rage of TRF7960 with metal near the antenna

    Christoph80 Christoph80
    Hello In our device a reader with TRF7960 is used to read ISO 15693 tags, which are placed 5cm below the antenna. This works fine. But when we place another PCB 5mm above the antenna, the tags can't be read anymore. I assume that the ground plane of the PCB causes this effect. When I activate...
    on Jan 20, 2012
  • Forum Post: RE: How to use TRF7970A read/write mifare classic

    G.M. G.M.
    Hi Eddie, could you please send me the source code of the project that will be used for read/write MIFARE Card? Is this software available for MSP430 and Stellaris M3/M4 as well? Which is the part number that you use for the project? it will be useful in order to understand the right size of memory...
    on May 9, 2012
  • Forum Post: TRF7960AEVM Controls the modulation depth

    Seishin Seishin
    Hi All, I am working on TRF7960EVM board. I want to change the modulation depth of ASK in the ISO15693 There is no change in the waveform I have the following settings on the GUI: ①Select COM Port ②Register settings    0x01 Register    B7=0    B6=1    B5=1    B4=0    B3=0    B2=0    B1...
    on May 16, 2012
  • Forum Post: TRF7960 Read Range using small antenna design

    Vladimir Nohava Vladimir Nohava
    Hello, Given the TRF7960EVM outputs 200mW of power and that the antenna diagonal length is 2" gives a reading range of 4". I am trying to design an antenna that can read laundry tags (RF-HDT-DVBE-N2) at a distance of up to 8 inches away. I see that the read distance using 300mmX300mm...
    on May 23, 2012
  • Forum Post: Inconsistent behavior of TRF7970?

    Anyu Dai Anyu Dai
    Hello guys in TI-Forum, I am now coding the RFID function with TRF7970's on 20 very identical PCB's offered by my HW colleague. I've imported my old codes for TRF7960 into this new project and made some changes, like SPI-edge, FIFO size, etc. The codes work well with the first and second...
    on May 31, 2012
  • Forum Post: MSP430 Programming

    prem m prem m
    Hi my name is Prem, I am working on a TRF 7960 EVM right now. I want to make some changes in the MSP430 program such that, we can send the data to another memory module when we connect the board to an external power supply and then we can retrieve the data when we connect the board to the computer. But...
    on Jul 16, 2012
  • Forum Post: How can I read multiple block from other RFID IC e.g. ICodeSL2 NXP?

    Hiro Hiro Hiro Hiro
    Hello, I am wiriting my own applicationwith C# and my requirement is to write 2 blocks of user memory. I have check with TI's GUI and it work well with TI transponder but I have problem when I change to other transponder with ICODE SL2. Do I need to modify somethig with TI's GUI? Or there is...
    on Aug 11, 2012
  • Forum Post: ISO14443 Air Interface Timing

    Vladimir Nohava Vladimir Nohava
    Hello, Do you have either measured or calculated ISO14443 A/B air interface timing like you have done for the ISO15693? I am currently using the trf7960 eval board. I would like to know the fastest possible read time for example the ISO15693 Read Single Block total time = 4.56mSec taken from your...
    on Aug 9, 2012
  • Forum Post: TRF7970 EVM failure reading Fujitsu MB89R118 tags

    tdyer tdyer
    I recently purchased a TRF7970 EVM board and I'm trying to read a Fujitsu MB89R118 that it is ISO15693 compliant. The inventory command fails along standard reads and writes. I can read other ISO15693 tags. I think it may be due to the Fujitsu requiring ASK 10% only. Any sample code or suggestions...
    on Aug 20, 2012
  • Forum Post: How to run in debug mode and distinguish two RFID tags in "Stand alone mode"?

    Henrik Zimmermann Henrik Zimmermann
    Hi I'm working on a project where I need the TRF7960EVM to work in "Stand alone mode" and detect if two or more 15693 tags are present. The indication can be very simple e.g. the LEDs on the EVM board. However the problem is to determine of there are more than one tag present. I have...
    on Aug 23, 2012
  • Forum Post: Where is the UID stored in source code for TRF7960/TRF7970 EVM

    Henrik Zimmermann Henrik Zimmermann
    The information obtained from the RFID tag seems to be stored in the variable "buf", which is an array with the length 300 and declared as unsigned 8 bit. In the code (ISO15693.c) there is a comment saying that "the first UID will be stored from buf[1] upwards", but a lot of other...
    on Aug 29, 2012
  • Forum Post: TRF7970A registers problems (same as in TRF7960) report

    Danko Ivanov Danko Ivanov
    Hi to all, This report could be usefull for many of you. Note that this was tested for SPI with SS only. Sincerely Danko Ivanov REPORT OF TRF7970A Registry problem I. Problem description NOTE! All data below are collected using SPI with SS. Other communications protocols ( parallel...
    on Oct 13, 2012
  • Forum Post: ICODE ILT ISO15693 3-mode-3

    Vladimir Nohava Vladimir Nohava
    Hello, Is there any TI reader that can support ICODE ILT which is based on ISO15693 3-mode-3, which is equivalent to UHF EPC Gen 2 class one protocol? Thanks Vlad
    on Oct 23, 2012
  • Forum Post: RE: RFID reader with TRF7960 and PIC24FJ128GA010

    javi garcia javi garcia
    Hi, How I can read the UID card HF-I standard? I communicate with the TRF7960, read their records, but I can not read the UID card, Can anybody help? thanks
    on Dec 20, 2012
  • Forum Post: RE: RFID reader with TRF7960 and PIC24FJ128GA010

    javi garcia javi garcia
    Hi Josh, I have adjusted both registers as you say, Chip Status Control Register and ISO Control the data sent by the SPI to configure the TRF7960 are: 0x20;0x20;0x00;0x00;0xC2;0x00;0x80;0x14;0x1F;0x31;0x40;0x87;0x3E I can read the chip the registers. buf I try to read the card I use this sequence...
    on Dec 20, 2012
  • Forum Post: RE: RFID reader with TRF7960 and PIC24FJ128GA010

    javi garcia javi garcia
    Josh- the flag IRQ is generated by the port 13 of the TRF7960???if so, I get no signal from it. sending data tells me you, and I hope that this terminal do a interruption on my micro, but it does, It don´t the rissing. Thank for all
    on Dec 21, 2012
  • Forum Post: RE: RFID reader with TRF7960 and PIC24FJ128GA010

    javi garcia javi garcia
    Hi Josh, Yes, i have a logic analyzer between MC and TRF7960, in the logic analyzer i can see the configuration register, when i send and read from the MCU, but, i can´t see the flag.
    on Dec 27, 2012
  • Forum Post: RE: RFID reader with TRF7960 and PIC24FJ128GA010

    javi garcia javi garcia
    javi garcia Hola Josh, Sí, tengo un analizador lógico entre MCU y TRF7960, en el analizador de lógica que se puede ver el registro de configuración, cuando i enviar y leer desde el MCU, pero no puedo ver la bandera. All time the IRQ is high, never it is low...
    on Dec 28, 2012
  • Forum Post: RE: RFID reader with TRF7960 and PIC24FJ128GA010

    javi garcia javi garcia
    Josh, I have the same result, the IQR is high. I use the TRF7960EVM, but i want to work directly with TRF7960, whitout MSP. My tag is HF-I standard, and only want read the UID Number I use the command of the http://www.ti.com/lit/ds/symlink/trf7960a.pdf (page 26).
    on Dec 28, 2012
  • Forum Post: Porting TRF79060A EVM code to TRF7970 board - Executing 15693 commands

    John Bullard John Bullard
    Hello, I'm relatively new to embedded development, apologies if this turns out to be a trivial fix. I've successfully ported most of my TRF7960A EVM firmware to my production board with a TRF7970 (+MSP430 2370). I'm able to carry out an inventory command and read 15693 UID's without...
    on Jan 22, 2013
  • Forum Post: Problem with TRF7970A EVB with ISO15693 (ICODE SLIX p/n: SL2S2002 from NXP) tag when two tags or more under read / write operation

    Wai CHing Cheuk Wai CHing Cheuk
    When one tags, can read and write using "TRF7970A_EVM_GUI" software. But cannot read // write when 2 tags or more, even the tags are placed very close to the antenna, and both tags is not placed on the same axis. (different placement for the tags already tried, pretty sure is the the RF problem...
    on Apr 12, 2013
  • Forum Post: Exchange of data between VCD and VICC while reading/writing multiple blocks

    Prasad Kulkarni1 Prasad Kulkarni1
    Hi, I am trying to calculate the time take by TRF796x reader to read multiple blocks from Tag using ISO15693 high data rate modulation. If i send command 23 (read multiple block) to read 64 blocks. I shall be sendind 6 byte + 8 byte of UID + EOF and SOF. After delay of ~ 0.32 ms, VICC shall respond...
    on Apr 25, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use