I wonder if you can help me? I am trying get the webserver demo running for the FRAM MSP430FR5735 board with the CC3000 module but I can’t get the standard code to compile.
Here is what I have done:
1) I downloaded the CC3000+FRAM Simple HTTP Web Server Application code from the Ti website (http://processors.wiki.ti.com/index.php/CC3000_Wi-Fi_Downloads) .
2) I unzipped & copied the code to my C:\ti\ folder where I created a directory called ‘Webserver’.
3) I opened up CSS5 and started a new project based on the MSP430FR5735 with the ‘blinky’ application. I compiled this application and everything was ok.
4) I then excluded ‘blinky’ from the build
5) I then imported the ‘demo.c’ file from the webserver directory into the project structure.
When I try and build the project I get a lot of errors thrown that it can’t find some (or most) of the included files (e.g. #include "wlan.h", #include "cc3000.h",#include "strlib.h".....).
If I change the include path to all of the locations that the flagged problems are located (which seems a very laborious task – is there a better way of doing this??) I still get problems that the project can’t build:
Description Resource Path Location Type
#171 expected a declaration webserv line 103, external location: C:\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#171 expected a declaration webserv line 103, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#171 expected a declaration webserv line 116, external location: C:\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#171 expected a declaration webserv line 116, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#171 expected a declaration webserv line 131, external location: C:\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#171 expected a declaration webserv line 131, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#171 expected a declaration webserv line 145, external location: C:\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#171 expected a declaration webserv line 145, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#171 expected a declaration webserv line 157, external location: C:\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#171 expected a declaration webserv line 157, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#171 expected a declaration webserv line 223, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 223, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 237, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 237, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 250, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 250, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 264, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 264, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 277, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 277, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 291, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 291, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 305, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 305, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#171 expected a declaration webserv line 71, external location: C:\lib\CC3000HostDriver\netapp.h C/C++ Problem
#171 expected a declaration webserv line 71, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\netapp.h C/C++ Problem
#171 expected a declaration webserv line 89, external location: C:\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#171 expected a declaration webserv line 89, external location: C:\lib\CC3000HostDriver\netapp.h C/C++ Problem
#171 expected a declaration webserv line 89, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#171 expected a declaration webserv line 89, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\netapp.h C/C++ Problem
#760 variable "hci_evnt_hdr_t" is not a type name webserv line 56, external location: C:\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#760 variable "hci_evnt_hdr_t" is not a type name webserv line 56, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#760 variable "netapp_pingreport_args_t" is not a type name webserv line 195, external location: C:\lib\CC3000HostDriver\netapp.h C/C++ Problem
#760 variable "netapp_pingreport_args_t" is not a type name webserv line 195, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\netapp.h C/C++ Problem
#760 variable "tNetappIpconfigRetArgs" is not a type name webserv line 237, external location: C:\lib\CC3000HostDriver\netapp.h C/C++ Problem
#760 variable "tNetappIpconfigRetArgs" is not a type name webserv line 237, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\netapp.h C/C++ Problem
#760 variable "tNetappIpconfigRetArgs" is not a type name webserv line 94, external location: C:\ti\Webserver\source\apps\MSP-EXP430FR5739\webserver\webserver\cc3000.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 107, external location: C:\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 107, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 122, external location: C:\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 122, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 136, external location: C:\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 136, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 148, external location: C:\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 148, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 160, external location: C:\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 160, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 228, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 228, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 241, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 241, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 255, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 255, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 268, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 268, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 282, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 282, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 296, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 296, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 310, external location: C:\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 310, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\hci.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 79, external location: C:\lib\CC3000HostDriver\netapp.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 79, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\netapp.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 94, external location: C:\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 94, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\evnt_handler.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 95, external location: C:\lib\CC3000HostDriver\netapp.h C/C++ Problem
#78-D this declaration has no storage class or type specifier webserv line 95, external location: C:\ti\Webserver\source\lib\CC3000HostDriver\netapp.h C/C++ Problem
Do you have any idea on where I am going wrong… am I importing the files/project incorrectly.
I am now completely out of ideas so any guidance on where I am going wrong & the best way to import existing projects into CCS5 will be appreciated.
Many thank.
Michael
Hi Michael,
I suggest that you import the project so that you get all the dependencies and settings correct.
Instructions:
Open CCS5
File->import
select Code Composer Studio -> Existing CCS/CCE Eclipse Projects.
Click next and then Browse to the project source folder you downloaded.
Select all the projects in Discovered Projects: list and click finish
This will import everything including project options and libraries.
Good luck
Hi Thanks for the information.... I tried that and I still get errors (Please see the screen grab)
Hi,
I was going off of general knowledge. I have never worked with this example before so I downloaded the source from http://www.ti.com/lit/zip/swrc246
and there is no CCS project files; just IAR.
Does anyone know if CCS is supported for this demo?
You can download http://www.ti.com/lit/zip/swrc235 which is the homeautomation project. It has CCS support. So you can try that and then use it as a CCS project reference for creating the HTTP demo.
It looks like the link on the download page still calls off just the IAR version (http://processors.wiki.ti.com/index.php/CC3000_Wi-Fi_Downloads) for the web server
I think I got the version for the CCS compiler from the E2E forum link …
http://e2e.ti.com/support/low_power_rf/f/851/p/187337/675485.aspx#675485
[Note: I have tried to compile this and it still doesn’t import & compile properly]
Towards the bottom of the page there was the following post from a Ti Employee with a link to a new CCS version of the web server demo–
Posted by Pedro5084
onJun 20, 2012 11:11 PM