Hi,
I am trying to interface CC3000 EM board with STM32F4 series micro.
i am following the "CC3000 Host Programming Guide" for the porting , testing and initial test setup.
The CC3000 initialization setup on host is as follows :
SPI baudrate : 1Mhz
CPOL : 0 CPHA : 1
In the CC3000 initilization process i am able to send the first command to CC3000 : Host ->> CC3000 - HCI_CMND_SIMPLE_LINK_START
The checked through the scope the MOSI line sends the data what it intends to send to CC3000, but as per the reference TI link i dont get the data on MISO :02 00 FF 00 00 00 00 00 00 00.
And neither CC3000 sends back command complete responses to host : HCI_CMND_SIMPLE_LINK_START
The IRQ doesnt go low after the command is sent from host to CC3000, so host continously polls for the response amd nevers comes out of the loop.
How could i verify if my CC3000 is working and the command i send is properly received by CC3000...????
Could any one tell me why CC3000 is not sending the response...??