I just purchased the following product for evaluation of the CC3000:
MSP-EXP430G2553 LaunchPad CC3000BOOST - SimpleLink™ Wi-Fi CC3000 BoosterPack
Product Number: MSP-EXP430G2-CC3000BOOST
I have been unable to establish network connectivity (or any connectivity) with this combination despite repeated attempts. The failure always occurs with First Configuration. MSP430 board jumpers are set to HW uart per instructions. This document was followed explicitly,
http://processors.wiki.ti.com/index.php/CC3000_Basic_Wi-Fi_example_application_for_Launchpad
Scenario follows:
(1) Patch Programmer, Launchpad - MSP430G2553 Patch Programmer Utility 1.11 was downloaded, installed and applied successfully,
http://processors.wiki.ti.com/index.php/CC3000_Wi-Fi_Downloads
(2) SDK 1.11 Windows was downloaded and installed (C:\ti\CC3000SDK\CC3000 SDK\MSP430G2553\Basic WiFi Application\...
(3) Under Start --> All programs --> CC3000 SDK --> MSP430G2553 --> Basic WiFi Appication --> (Execute) Download Basic WiFi Binary
(4) Output from Step (3)
Please ensure that your FRAM board is configured correctly and that its USB cable is connected. Press any key to continue . . .
C:\ti\CC3000SDK\CC3000 SDK\MSP430G2553\Basic WiFi Application\tools\MSP430Flashe r_1.1.3>MSP430Flasher.exe -n MSP430G2553 -w "../Binary\BasicWiFiApplication.txt" -z [VCC] -v -g
Evaluating additional triggers...done
Initializing interface on TIUSB port...done
Checking firmware compatibility...done
Reading FW version...done
Reading HW version...done
Powering up...done
Configuring...done
Accessing device...done
Reading device information...done
Loading file into device...done
Verifying transfer...done
Resetting device...done
Refreshing registers... /* ---------------------------------------------------------------------------- * UseCase : MSP430Flasher.exe * Arguments : -n MSP430G2553 -w ../Binary\BasicWiFiApplication.txt -z [VCC] - v -g
* ATTENTION: Default options used due to invalid argument list. * ---------------------------------------------------------------------------- * Driver :
loaded * Dll Version : 20409001 * FwVersion : 30394216 * Interface : TIUSB * HwVersion : E 2.0 * Mode : AUTO * Device : MSP430G2xx3 * EEM : Level 1, ClockCntrl 1 * Prog.File : ../Binary\BasicWiFiApplication.txt (ERASE_ALL, verified = TRUE) * BSL Unlock : FALSE * InfoA Access: FALSE * VCC ON : TRUE * UseCase specific tasks: ----------------------------------------------------
* Powering up...done
* Disconnecting from device... * ----------------------------------------------------------------------------
* Driver : closed (No error) * ---------------------------------------------------------------------------- */
Please look above to ensure all steps were performed successfully. LED1 of the FRAM board should have turned on if the CC3000 EM Module is mounted. Press any key to continue . . .
(5) The result from Step (3) is MSP green and red LED on.
(6) Putty is unable to communicate for first configuration. Power cycling doesn't help. the USB COM port is ok because it was tested with the hardware UART on MSP430 talking to Putty to turn the red and green LEDs on/off.
(7) The same result occurs when the Basic WiFi App Source is compiled with Code Composer.
(8) It appears to me that the code supplied for the MSPG2553 Value Line board is incorrect. Note the comment on the download binary output above, "Please ensure that your FRAM board" ... The MSP430G2553 is not a FRAM board. Any suggestions to get going are gratefully appreciated.
Baxter