All,
I have two sets of hardware.
A.) The CC3000EM with the MSP-EXP430FR5739.
B.) Our custom PCB with the CC3000 controlled by an Atmel AVR.
I am trying to get up to speed on as fast as possible with all the details that I need to know for the development on my custom board.
1.) I have started off spending some time with the EVM (CC3000EM & MSP-EXP430FR5739) using the basic wifi application, using the SmartConfig tool on my ipad, and send/receiving UDP data. I don't know what else I can do with the EVM at this point. I mainly wanted to verify my access point works correctly and the Smartconfig works correctly with the ipad.
2.) I am now at a point where I believe it makes sense to start working with my custom board. I would like to verify that the CC3000 works correctly, I can connect to an access point and send data back and forth from the module without spending the time right now to have all the code written for my AVR. I want to verify the hardware is working correctly before I jump into some time consuming software development. If I set the jumpers so the CC3000 is in test mode should I be able to do all of this? I have a header on the board for the connections to the WL_RS232_TX and WL_RS232_RX. I also have a FTDI USB to TTL serial cable for this connection.
3.) I am also at a point where I need to read all the documentation at:
http://processors.wiki.ti.com/index.php/CC3000
Is it fair to said that I should basically read all the information here?
4.) Any other tips or suggestions to make this ride a little less bumpy? :)
Thank you very much.
-Mike