Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: FAQ: Access protection of the CC111x/CC243x/CC251x FLASH memory by 611949
Access protection of the FLASH memory is done via designated bits in the Flash Information Page.This can be done only through the designated CC111x/CC243x/CC251x debug interface.For read protection the DBGLOCK bit must be set. This will disable all access to the FLASH memorythrough the debug interface.For write protection the lock size bits LSIZE[2:0] must be used, along with the BBLOCK lock bit,which also offers write protection of the boot sector page.