Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
The CC1020 RF transceiver is very easy to interface with a microcontroller. The chip is configured using a four-wire bus, comprising of PCLK, PDI, PDO and PSEL signals. Data interfacing is done via the DCLK and DIO pins. Data decision and synchronisation is done by the CC1020, easing the workload of the microcontroller considerably. Using the synchronous Manchester or NRZ modes, the CC1020 supplies a synchronous clock, which can be used for triggering interrupts in the microcontroller, or for interfacing with a synchronous serial interface. This application note covers interfacing the CC1020 to microcontrollers. Information is given about both the configuration and data interfaces of the CC1020.
http://www.ti.com/litv/pdf/swra069Download associated code files