Q: FAQ: Binding (Z-Stack, ZigBee) by 656199

Changed binding in 1.4.0

In ZigBee-2006 the previously defined coordinator binding has been obfuscated. Our Z-Stack 1.4.0 release, which is ZigBee-2006 compliant, has been written according to specification, although we do provide backward compatibility via compile options to utilize this feature. However the elimination of Coordinator Binding means that binding entries are no longer kept on the Coordinator, and instead are stored locally on devices. For more information on binding please see the Developer’s Guide provided as part of the 1.4.1 or later release.