Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: FAQ: Clocking the 32 kHz oscillator externally
The 32 kHz oscillator is designed with a differential input so to get optimum results one should drive both XOSC32_Q1 and XOSC32_Q2 with one of them being the inverted of the other.
The duty cycle should be within the 30-70% range.The amplitude of the input signal should ideally be rail-to-rail.Frequency should be in the 10-40 kHz range