Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
This is the Low Power RF Design Notes section. You'll find application notes, valuable forum posts, FAQ and design notes in the sections below.
With the large number of design notes available, search is an effective tool to help you reach the most helpful information.
You can also browse our techincial documentation here.
If you have questions related to the documents listed in this section, thank you for posting your question in the appropriate E2E forum.
Hi All,
when i am compile, i am getting this error 1) Fatal Error[Pe1696]: cannot open source file "msp430f6779.h" D:\IAR_project\CODE_MSP430F6XX\MSP430F67xx_MSP430F67xx1_Code_Examples\C\MSP430F677x_SD24B_02.c 88
searched: "C:\Program Files\IAR Systems\Embedded Workbench 6.0\430\inc\dlib\.\"
MSP430F677x_SD24B_02.c
Fatal Error[Pe1696]: cannot open source file "msp430f6779.h" D:\IAR_project\CODE_MSP430F6XX\MSP430F67xx_MSP430F67xx1_Code_Examples\C\MSP430F677x_SD24B_02.c 88
searched: "C:\Program Files\IAR Systems\Embedded Workbench 6.0\430\inc\dlib\..\"
searched: "C:\Program Files\IAR Systems\Embedded Workbench 6.0\430\inc\dlib\c\"
Error while running C/C++ compiler
regards
RAvi
Hello E2E,
I am currently have such question on these module PAN1720 (CC2540 IC) , I would like to know that the power supply decoupling for the PAN1720 module. Will a single 47uf bypass capacitor connected to the GND and a ferrite in series with our 3.3v battery's output be sufficient?
Or do we need two 47uf capacitors along with a ferrite as per the attached example circuit which is from the PAN 1720 Application guide
www.pideu.panasonic.de/.../168ApplicationNote.pdf (page 5)?
Thanks and Best regards.