Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
This document describes a PCB antenna designed for 2.4 GHz operation. The antenna is an IP based solution from Pinyon and can be used with all transceivers and transmitters from Texas Instruments, which operates in the 2.4 GHz frequency band. Maximum gain is measured to be 6.33 dBi and the antenna size is 35 x 80 mm. Figure 1 shows a picture of the reference design using CC2510 and the Pinyon antenna. The EM board is designed to be used with the SmartRF04 ® board.
http://www.ti.com/lit/swra254