Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
The purpose of this design note is to show how to optimize the current consumption for a polling receiver based on some of the digital features of the CC1100, CC1101 and CC2500, such as WOR and RSSI.
The design note will also show how a polling receiver can be implemented using the CC1110/CC1111Fx and CC2510/CC2511Fx. This design note will assume that the reader is familiar with the WOR functionality of the CC1100, CC1101 and CC2500. Details on WOR can be found in AN047.
http://www.ti.com/lit/swra207Download associated code files