Welcome to the Low Power RF & Wireless Connectivity Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: FAQ: Strobe command SPI timing for CC110x/CC1150/CC2500/CC2550 by 611949
A Strobe command can be issued immediately after the preceeding Strobe command, provided that the preceeding Strobe commandhas been completely transfered over the SPI interface. However, note that for SPI clock speed above 6.5 MHz, the CC110x SPI interfacerequires a certain delay between each SPI byte transfer (see the respective Data Sheets).