The TMS320C2000 Piccolo multi-day workshop is a hands-on technical course facilitated by qualified Texas Instruments' instructors. This workshop will cover the Piccolo F2803x devices, which are the latest members of the C2000 MCU family. The workshop steps the user through system initialization, peripheral setup and programming an application into flash memory using the Flash Plug-in utility. Topics also included are IQmath, the CLA, and DSP/BIOS.

Every lab exercise builds on the previous lab exercise, running a common application theme throughout the workshop.  The lab exercises are performed using the F28035 Piccolo Experimenter's Kit.  This kit consists of a docking station and an F28035 ControlCARD.  The docking station features on-board USB JTAG emulation, access to all of the ControlCARD signals/peripherals, and breadboard areas.  The ControlCARD is a complete board level module that utilizes an industry-standard DIMM form factor to provide a single-board controller solution.  The docking station is fully powered from the USB connection and no external power supply is needed. 

All workshop attendees will receive a free Piccolo F28035 Experimenter's Kit to help reinforce the workshop concepts after the class is over. 

          Tuesday, Mar 16 – Thursday, Mar 18

Register Now!