LAUNCHXL-F28379D Rev1.2: Layout error causing signal contention on ADC channels

Hello E2E community, 

TI recently discovered an issue with the LAUNCHXL-F28379D LaunchPad. This issue affects all LaunchPads marked VER: 1.1 and impacts the ability to utilize all of the available ADC channels.

 

The affected LaunchPads has ADCINA2 shorted to VREFHIB. This error was caused by a via intersecting a trace. It is recommended that users avoid using ADCINA2. 

Additionally, manufacturing tolerance variation may cause a short between U1.VIN+ and ADCINB4 or ADCINC4. No issues have been reported on actual hardware, but it is worth noting in case odd behavior is observed.

ADCINA2/VREFHIB contention:

U1.VIN+/ADCINB4/ADCINC4 contention:

  

These errors will be corrected in a future revision of the LaunchPad. Also, additional modifications to the board design will provide a more flexible evaluation platform for the user. We apologize for any inconvenience this may have caused.  Thank you for evaluating our TMS320F28379D MCU!

Did a reply answer your question? If yes, please click the "Verify Answer" button located at the bottom of that post.
Visit these helpful C2000 Links!
C2000 TI Wiki Pages
TI Forum Sitemap
C2000Ware
ControlSUITE

C2000 Getting Started
CLA FAQs
Workshop Material!
LaunchPads

7 Replies