This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] MotorWare v18 Release

Motorware v18 has officially been released. Find some of the changes enumerated below:

  • HAL_setTrigger() change to fix issue where when USER_NUM_PWM_TICKS_PER_ISR_TICK was set to 2 or 3, and ISR execution time was less than half of ISR period, ADC trigger would sometimes be missed
  • Fixed issue in GPIO_setPortData() for F2805x that had incorrect parameter data width
  • Fixed usDelay() issues in all hal.c files, replaced with US_TO_CNT() macro
  • Fixed CMP saturation limit in HAL_WritePwmData() in hal.h for F2805x only, changed lower limit from _IQ(0.0) to 1
  • Update PWM_setSocAPulseSrc() in all pwm.c
  • Remove OVM functions in lab5h and remove svgen_current.c file in project
  • Fixed compiler error in hal.h for 06x projects with HVKit due to an error in #ifdef statement for HALL GPIO pin numbers
  • Fixed LED blinking timing error in main_ISR() for all FOC and MOTION files that have toggle led code (New Enhancement)
  • Changed the argument of CPU_USAGE_setParams() to variable instead of fixed timer period since timer period was changed in hal.c in MW17. Affects labs: 03b, 07, 11a, and 11b (these labs use the legacy CPU_USAGE module)
  • Changed the argument of FEM_setParams() to variable instead of fixed timer period since timer period was changed in hal.c in MW17. Affects labs: 03b, 07
  • Changed motor definition to resolve compiler error when using IPD projects in the below user.h files:
    • \boostxldrv8305_revA\28x\f2806xF\src\user_j1.h
    • \boostxldrv8305_revA\28x\f2806xF\src\user_j5.h

  • All functions running in main_ISR() in lab11x were added to “ramfunc” for reducing cycle time (New Enhancement)
  • Added lab07 and lab09 project for BoostXL-DRV8305 + F2806x  "boostxldrv8305_revA\f28x\f2806xF\projects\ccs"
  • Added Volt/Hertz module in modules/vs_freq/src directory. This module generates an output command voltage for a specific input command frequency according to the specified volts/hertz profile.
  • Added Angle Generator module in modules/angle_gen/src directory. This module generates angle output for a specific input command frequency.
  • Added proj_01b project for all kits and controllers.
  • Added proj_01c project for all kits and controllers.
  • Added gMotorVars[HAL_MTR2].CtrlVersion = version; to lab10d for bug fix
  • Relocated CLK_disableTbClockSync() to before timebase, compare control, action qualifier, dead band and trip zone initialization loops. This was done to fix issue where PWM sync could sometimes be lost when hard-resetting MCU
  • Changed RsRecalc functionality to have initial value of USER_MOTOR_Rs instead of 0, which will allow quicker settling time
  • Offsets removed from user_2motors.h to avoid issue where current/voltage offsets were defined in two separate header files
  • Added definition for updateRsOnLine() for lab11a, takes EST_Handle parameter instead of CTRL_Handle parameter as expected by runRsOnLine() in lab07
  • Added spi.c and drv8301.c source files to all F2802xF LaunchPad projects that were designed for DRV8301 BoosterPack

Sean

Did a reply answer your question? If yes, please click the "Verify Answer" button located at the bottom of that post.
Visit these helpful C2000 Links!

C2000 TI Wiki Pages
TI Forum Sitemap
ControlSUITE
C2000 Getting Started
CLA FAQs
Workshop Material!

32 Replies

  • In reply to Maria Todorova:

    Same problem here.

    Windows 10 Enterprise

    Thank you.

    Radu

  • In reply to Radu Iorgulescu80:

    I seem to have fixed the problem by uninstalling Motrware and re-installing it taking all the defaults (previously I was specifying the install directory which might be the reason why it couldn't find its projects...)
    Radu

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.