This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TMS320F28335: compacting the sections of the flash memory to create a bootloader

Prodigy 200 points

Replies: 7

Views: 195

Part Number: TMS320F28335

hello,
i am trying to develop a new bootloader for my TMS320F2833 that resides on a Delfino evaluation board and manages a current software and an updated software. in my project the flash memory is segmented into 8 sections and is organized as follows:
the first section contains the botloader.
the sections 2 3 4 contain the current software image.
the sections 5 6 7 contain the updated software image.
my bootloader chooses what software to run at the start up of the system.
could you please give me any suggestions on how to rework the linker file to compact the sections 2 3 4 (make them adjacent) to contain the current software image and the sections 5 6 7 to contain the update software image? also any suggestion on how to verify that my current software size can be contained in those sections? following you can find my linker file that is arranged to contain just one program without bootloader.

MEMORY
{
PAGE 0:    /* Program Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */

   ZONE0       : origin = 0x004000, length = 0x001000     /* XINTF zone 0 */
   RAML0       : origin = 0x008000, length = 0x001000     /* on-chip RAM block L0 */
   RAML1       : origin = 0x009000, length = 0x001000     /* on-chip RAM block L1 */
   RAML2       : origin = 0x00A000, length = 0x001000     /* on-chip RAM block L2 */
   RAML3       : origin = 0x00B000, length = 0x001000     /* on-chip RAM block L3 */
   ZONE6       : origin = 0x0100000, length = 0x100000    /* XINTF zone 6 */
   ZONE7A      : origin = 0x0200000, length = 0x00FC00    /* XINTF zone 7 - program space */
   FLASHH      : origin = 0x300000, length = 0x008000     /* on-chip FLASH */
   FLASHG      : origin = 0x308000, length = 0x008000     /* on-chip FLASH */
   FLASHF      : origin = 0x310000, length = 0x010000     /* on-chip FLASH */
/*   FLASHE      : origin = 0x318000, length = 0x008000      on-chip FLASH */
   FLASHD      : origin = 0x320000, length = 0x008000     /* on-chip FLASH */
   FLASHC      : origin = 0x328000, length = 0x008000     /* on-chip FLASH */
   FLASHA      : origin = 0x338000, length = 0x007F80     /* on-chip FLASH */
   CSM_RSVD    : origin = 0x33FF80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
   BEGIN       : origin = 0x33FFF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
   CSM_PWL     : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
   OTP         : origin = 0x380400, length = 0x000400     /* on-chip OTP */
   ADC_CAL     : origin = 0x380080, length = 0x000009     /* ADC_cal function in Reserved memory */
   
   IQTABLES    : origin = 0x3FE000, length = 0x000b50     /* IQ Math Tables in Boot ROM */
   IQTABLES2   : origin = 0x3FEB50, length = 0x00008c     /* IQ Math Tables in Boot ROM */  
   FPUTABLES   : origin = 0x3FEBDC, length = 0x0006A0     /* FPU Tables in Boot ROM */
   ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */        
   RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
   VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */

PAGE 1 :   /* Data Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
           /* Registers remain on PAGE1                                                  */
   
   BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
   RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
   RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   RAML4       : origin = 0x00C000, length = 0x001000     /* on-chip RAM block L4 */
   RAML5       : origin = 0x00D000, length = 0x001000     /* on-chip RAM block L5 */
   RAML6       : origin = 0x00E000, length = 0x001000     /* on-chip RAM block L6 */
   RAML7       : origin = 0x00F000, length = 0x001000     /* on-chip RAM block L7 */
   ZONE7B      : origin = 0x20FC00, length = 0x000400     /* XINTF zone 7 - data space */
   FLASHB      : origin = 0x330000, length = 0x008000     /* on-chip FLASH */
}

/* Allocate sections to memory blocks.
   Note:
         codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
                   execution when booting to flash
         ramfuncs  user defined section to store functions that will be copied from Flash into RAM
*/
 
SECTIONS
{
 
   /* Allocate program areas: */
   .cinit              : > FLASHA      PAGE = 0
   .pinit              : > FLASHA      PAGE = 0
   .text               : > FLASHF      PAGE = 0
   codestart           : > BEGIN       PAGE = 0
   ramfuncs            : LOAD = FLASHD,
                         RUN = RAML0,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         PAGE = 0

   csmpasswds          : > CSM_PWL     PAGE = 0
   csm_rsvd            : > CSM_RSVD    PAGE = 0
   
   /* Allocate uninitalized data sections: */
   .stack              : > RAMM1       PAGE = 1
   .ebss               : > RAML4       PAGE = 1
   .esysmem            : > RAMM1       PAGE = 1

   .sysmem             : > RAML6       PAGE = 1
   .cio                : > RAML6       PAGE = 1

   /* Initalized sections go in Flash */
   /* For SDFlash to program these, they must be allocated to page 0 */
   .econst             : > FLASHC      PAGE = 0
   .switch             : > FLASHC      PAGE = 0

   /* Allocate IQ math areas: */
   IQmath              : > FLASHC      PAGE = 0                  /* Math Code */
   IQmathTables        : > IQTABLES,   PAGE = 0, TYPE = NOLOAD
   
   /* Uncomment the section below if calling the IQNexp() or IQexp()
      functions from the IQMath.lib library in order to utilize the
      relevant IQ Math table in Boot ROM (This saves space and Boot ROM
      is 1 wait-state). If this section is not uncommented, IQmathTables2
      will be loaded into other memory (SARAM, Flash, etc.) and will take
      up space, but 0 wait-state is possible.
   */
   /*
   IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
   {
   
              IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
   
   }
   */
   
   FPUmathTables    : > FPUTABLES, PAGE = 0, TYPE = NOLOAD
         
   /* Allocate DMA-accessible RAM sections: */
   DMARAML4         : > RAML4,     PAGE = 1
   DMARAML5         : > RAML5,     PAGE = 1
   DMARAML6         : > RAML6,     PAGE = 1
   DMARAML7         : > RAML7,     PAGE = 1
   
   /* Allocate 0x400 of XINTF Zone 7 to storing data */
   ZONE7DATA        : > ZONE7B,    PAGE = 1

   /* .reset is a standard section used by the compiler.  It contains the */
   /* the address of the start of _c_int00 for C Code.   /*
   /* When using the boot ROM this section and the CPU vector */
   /* table is not needed.  Thus the default type is set here to  */
   /* DSECT  */
   .reset              : > RESET,      PAGE = 0, TYPE = DSECT
   vectors             : > VECTORS     PAGE = 0, TYPE = DSECT
   
   /* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */
   .adc_cal     : load = ADC_CAL,   PAGE = 0, TYPE = NOLOAD

}

/*
//===========================================================================
// End of file.
//===========================================================================
*/



best regards

  •  Dear Marcello, 

    Everything you need to know about linker command files is available here and here:

    Please study the details and do the related exercises in Module 2 of the training material available here.

    After you have reviewed this material, please let us know if you have any additional questions.

    Cheers!  Krishna 

  • In reply to Krishna Allam:

    hello,

    i succeeded in compacting my flash sections to contain the software image in a section large 0x18000. now, i am trying to make the software relocatable by using the related in advanced options->linker output. neverthless, i get many errors of the following type:

    program will not fit into memory.

    this happen for registers sections that should be allocated at fixed and not modifiable addresses in data memory as it can be seen in the attached snapshots (registers with red baloon do not fit into memory) so an enlargement of the size of the sections in the linker file is not a good idea. also, i tried to optimize the code by setting the level equal to 5 but it does not work, too.

    any idea on how to solve this issue?thanks a lot.

    attached my linker file

    MEMORY

    {

    PAGE 0:    /* Program Memory */

    PAGE 1:    /* Data Memory */

      DEV_EMU     : origin = 0x000880, length = 0x000180     /* device emulation registers */

      FLASH_REGS  : origin = 0x000A80, length = 0x000060     /* FLASH registers */

      CSM         : origin = 0x000AE0, length = 0x000010     /* code security module registers */

      ADC_MIRROR  : origin = 0x000B00, length = 0x000010     /* ADC Results register mirror */

      XINTF       : origin = 0x000B20, length = 0x000020     /* external interface registers */

      CPU_TIMER0  : origin = 0x000C00, length = 0x000008     /* CPU Timer0 registers */

      CPU_TIMER1  : origin = 0x000C08, length = 0x000008     /* CPU Timer0 registers (CPU Timer1 & Timer2 reserved TI use)*/

      CPU_TIMER2  : origin = 0x000C10, length = 0x000008     /* CPU Timer0 registers (CPU Timer1 & Timer2 reserved TI use)*/

      PIE_CTRL    : origin = 0x000CE0, length = 0x000020     /* PIE control registers */

      PIE_VECT    : origin = 0x000D00, length = 0x000100     /* PIE Vector Table */

      DMA         : origin = 0x001000, length = 0x000200     /* DMA registers */

      MCBSPA      : origin = 0x005000, length = 0x000040     /* McBSP-A registers */

      MCBSPB      : origin = 0x005040, length = 0x000040     /* McBSP-B registers */

      ECANA       : origin = 0x006000, length = 0x000040     /* eCAN-A control and status registers */

      ECANA_LAM   : origin = 0x006040, length = 0x000040     /* eCAN-A local acceptance masks */

      ECANA_MOTS  : origin = 0x006080, length = 0x000040     /* eCAN-A message object time stamps */

      ECANA_MOTO  : origin = 0x0060C0, length = 0x000040     /* eCAN-A object time-out registers */

      ECANA_MBOX  : origin = 0x006100, length = 0x000100     /* eCAN-A mailboxes */

      ECANB       : origin = 0x006200, length = 0x000040     /* eCAN-B control and status registers */

      ECANB_LAM   : origin = 0x006240, length = 0x000040     /* eCAN-B local acceptance masks */

      ECANB_MOTS  : origin = 0x006280, length = 0x000040     /* eCAN-B message object time stamps */

      ECANB_MOTO  : origin = 0x0062C0, length = 0x000040     /* eCAN-B object time-out registers */

      ECANB_MBOX  : origin = 0x006300, length = 0x000100     /* eCAN-B mailboxes */

      EPWM1       : origin = 0x006800, length = 0x000022     /* Enhanced PWM 1 registers */

      EPWM2       : origin = 0x006840, length = 0x000022     /* Enhanced PWM 2 registers */

      EPWM3       : origin = 0x006880, length = 0x000022     /* Enhanced PWM 3 registers */

      EPWM4       : origin = 0x0068C0, length = 0x000022     /* Enhanced PWM 4 registers */

      EPWM5       : origin = 0x006900, length = 0x000022     /* Enhanced PWM 5 registers */

      EPWM6       : origin = 0x006940, length = 0x000022     /* Enhanced PWM 6 registers */

      ECAP1       : origin = 0x006A00, length = 0x000020     /* Enhanced Capture 1 registers */

      ECAP2       : origin = 0x006A20, length = 0x000020     /* Enhanced Capture 2 registers */

      ECAP3       : origin = 0x006A40, length = 0x000020     /* Enhanced Capture 3 registers */

      ECAP4       : origin = 0x006A60, length = 0x000020     /* Enhanced Capture 4 registers */        

      ECAP5       : origin = 0x006A80, length = 0x000020     /* Enhanced Capture 5 registers */        

      ECAP6       : origin = 0x006AA0, length = 0x000020     /* Enhanced Capture 6 registers */        

      EQEP1       : origin = 0x006B00, length = 0x000040     /* Enhanced QEP 1 registers */

      EQEP2       : origin = 0x006B40, length = 0x000040     /* Enhanced QEP 2 registers */  

      GPIOCTRL    : origin = 0x006F80, length = 0x000040     /* GPIO control registers */

      GPIODAT     : origin = 0x006FC0, length = 0x000020     /* GPIO data registers */

      GPIOINT     : origin = 0x006FE0, length = 0x000020     /* GPIO interrupt/LPM registers */

      SYSTEM      : origin = 0x007010, length = 0x000020     /* System control registers */

      SPIA        : origin = 0x007040, length = 0x000010     /* SPI-A registers */

      SCIA        : origin = 0x007050, length = 0x000010     /* SCI-A registers */

      XINTRUPT    : origin = 0x007070, length = 0x000010     /* external interrupt registers */

      ADC         : origin = 0x007100, length = 0x000020     /* ADC registers */

      SCIB        : origin = 0x007750, length = 0x000010     /* SCI-B registers */

      SCIC        : origin = 0x007770, length = 0x000010     /* SCI-C registers */

      I2CA        : origin = 0x007900, length = 0x000040     /* I2C-A registers */

      CSM_PWL     : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations. */

      PARTID      : origin = 0x380090, length = 0x000001     /* Part ID register location */

    }

    SECTIONS

    {

      PieVectTableFile : > PIE_VECT,   PAGE = 1

    /*** Peripheral Frame 0 Register Structures ***/

      DevEmuRegsFile    : > DEV_EMU,     PAGE = 1

      FlashRegsFile     : > FLASH_REGS,  PAGE = 1

      CsmRegsFile       : > CSM,         PAGE = 1

      AdcMirrorFile     : > ADC_MIRROR,  PAGE = 1

      XintfRegsFile     : > XINTF,       PAGE = 1

      CpuTimer0RegsFile : > CPU_TIMER0,  PAGE = 1

      CpuTimer1RegsFile : > CPU_TIMER1,  PAGE = 1

      CpuTimer2RegsFile : > CPU_TIMER2,  PAGE = 1  

      PieCtrlRegsFile   : > PIE_CTRL,    PAGE = 1    

      DmaRegsFile       : > DMA,         PAGE = 1

    /*** Peripheral Frame 3 Register Structures ***/

      McbspaRegsFile    : > MCBSPA,      PAGE = 1

      McbspbRegsFile    : > MCBSPB,      PAGE = 1

    /*** Peripheral Frame 1 Register Structures ***/

      ECanaRegsFile     : > ECANA,       PAGE = 1

      ECanaLAMRegsFile  : > ECANA_LAM    PAGE = 1  

      ECanaMboxesFile   : > ECANA_MBOX   PAGE = 1

      ECanaMOTSRegsFile : > ECANA_MOTS   PAGE = 1

      ECanaMOTORegsFile : > ECANA_MOTO   PAGE = 1

      ECanbRegsFile     : > ECANB,       PAGE = 1

      ECanbLAMRegsFile  : > ECANB_LAM    PAGE = 1  

      ECanbMboxesFile   : > ECANB_MBOX   PAGE = 1

      ECanbMOTSRegsFile : > ECANB_MOTS   PAGE = 1

      ECanbMOTORegsFile : > ECANB_MOTO   PAGE = 1

      EPwm1RegsFile     : > EPWM1        PAGE = 1  

      EPwm2RegsFile     : > EPWM2        PAGE = 1  

      EPwm3RegsFile     : > EPWM3        PAGE = 1  

      EPwm4RegsFile     : > EPWM4        PAGE = 1  

      EPwm5RegsFile     : > EPWM5        PAGE = 1  

      EPwm6RegsFile     : > EPWM6        PAGE = 1

      ECap1RegsFile     : > ECAP1        PAGE = 1  

      ECap2RegsFile     : > ECAP2        PAGE = 1  

      ECap3RegsFile     : > ECAP3        PAGE = 1  

      ECap4RegsFile     : > ECAP4        PAGE = 1

      ECap5RegsFile     : > ECAP5        PAGE = 1  

      ECap6RegsFile     : > ECAP6        PAGE = 1

      EQep1RegsFile     : > EQEP1        PAGE = 1  

      EQep2RegsFile     : > EQEP2        PAGE = 1              

      GpioCtrlRegsFile  : > GPIOCTRL     PAGE = 1

      GpioDataRegsFile  : > GPIODAT      PAGE = 1

      GpioIntRegsFile   : > GPIOINT      PAGE = 1

    /*** Peripheral Frame 2 Register Structures ***/

      SysCtrlRegsFile   : > SYSTEM,      PAGE = 1

      SpiaRegsFile      : > SPIA,        PAGE = 1

      SciaRegsFile      : > SCIA,        PAGE = 1

      XIntruptRegsFile  : > XINTRUPT,    PAGE = 1

      AdcRegsFile       : > ADC,         PAGE = 1

      ScibRegsFile      : > SCIB,        PAGE = 1

      ScicRegsFile      : > SCIC,        PAGE = 1

      I2caRegsFile      : > I2CA,        PAGE = 1

    /*** Code Security Module Register Structures ***/

      CsmPwlFile        : > CSM_PWL,     PAGE = 1

    /*** Device Part ID Register Structures ***/

      PartIdRegsFile    : > PARTID,      PAGE = 1

    }

    /*

    //===========================================================================

    // End of file.

    //===========================================================================

    */

  • In reply to marcello ioppolo1:

    folliwing the linker file that contains the sections with the errors:
    MEMORY
    {
    PAGE 0: /* Program Memory */

    PAGE 1: /* Data Memory */

    DEV_EMU : origin = 0x000880, length = 0x000180 /* device emulation registers */
    FLASH_REGS : origin = 0x000A80, length = 0x000060 /* FLASH registers */
    CSM : origin = 0x000AE0, length = 0x000010 /* code security module registers */

    ADC_MIRROR : origin = 0x000B00, length = 0x000010 /* ADC Results register mirror */

    XINTF : origin = 0x000B20, length = 0x000020 /* external interface registers */

    CPU_TIMER0 : origin = 0x000C00, length = 0x000008 /* CPU Timer0 registers */
    CPU_TIMER1 : origin = 0x000C08, length = 0x000008 /* CPU Timer0 registers (CPU Timer1 & Timer2 reserved TI use)*/
    CPU_TIMER2 : origin = 0x000C10, length = 0x000008 /* CPU Timer0 registers (CPU Timer1 & Timer2 reserved TI use)*/

    PIE_CTRL : origin = 0x000CE0, length = 0x000020 /* PIE control registers */
    PIE_VECT : origin = 0x000D00, length = 0x000100 /* PIE Vector Table */

    DMA : origin = 0x001000, length = 0x000200 /* DMA registers */

    MCBSPA : origin = 0x005000, length = 0x000040 /* McBSP-A registers */
    MCBSPB : origin = 0x005040, length = 0x000040 /* McBSP-B registers */

    ECANA : origin = 0x006000, length = 0x000040 /* eCAN-A control and status registers */
    ECANA_LAM : origin = 0x006040, length = 0x000040 /* eCAN-A local acceptance masks */
    ECANA_MOTS : origin = 0x006080, length = 0x000040 /* eCAN-A message object time stamps */
    ECANA_MOTO : origin = 0x0060C0, length = 0x000040 /* eCAN-A object time-out registers */
    ECANA_MBOX : origin = 0x006100, length = 0x000100 /* eCAN-A mailboxes */

    ECANB : origin = 0x006200, length = 0x000040 /* eCAN-B control and status registers */
    ECANB_LAM : origin = 0x006240, length = 0x000040 /* eCAN-B local acceptance masks */
    ECANB_MOTS : origin = 0x006280, length = 0x000040 /* eCAN-B message object time stamps */
    ECANB_MOTO : origin = 0x0062C0, length = 0x000040 /* eCAN-B object time-out registers */
    ECANB_MBOX : origin = 0x006300, length = 0x000100 /* eCAN-B mailboxes */

    EPWM1 : origin = 0x006800, length = 0x000022 /* Enhanced PWM 1 registers */
    EPWM2 : origin = 0x006840, length = 0x000022 /* Enhanced PWM 2 registers */
    EPWM3 : origin = 0x006880, length = 0x000022 /* Enhanced PWM 3 registers */
    EPWM4 : origin = 0x0068C0, length = 0x000022 /* Enhanced PWM 4 registers */
    EPWM5 : origin = 0x006900, length = 0x000022 /* Enhanced PWM 5 registers */
    EPWM6 : origin = 0x006940, length = 0x000022 /* Enhanced PWM 6 registers */

    ECAP1 : origin = 0x006A00, length = 0x000020 /* Enhanced Capture 1 registers */
    ECAP2 : origin = 0x006A20, length = 0x000020 /* Enhanced Capture 2 registers */
    ECAP3 : origin = 0x006A40, length = 0x000020 /* Enhanced Capture 3 registers */
    ECAP4 : origin = 0x006A60, length = 0x000020 /* Enhanced Capture 4 registers */
    ECAP5 : origin = 0x006A80, length = 0x000020 /* Enhanced Capture 5 registers */
    ECAP6 : origin = 0x006AA0, length = 0x000020 /* Enhanced Capture 6 registers */

    EQEP1 : origin = 0x006B00, length = 0x000040 /* Enhanced QEP 1 registers */
    EQEP2 : origin = 0x006B40, length = 0x000040 /* Enhanced QEP 2 registers */

    GPIOCTRL : origin = 0x006F80, length = 0x000040 /* GPIO control registers */
    GPIODAT : origin = 0x006FC0, length = 0x000020 /* GPIO data registers */
    GPIOINT : origin = 0x006FE0, length = 0x000020 /* GPIO interrupt/LPM registers */

    SYSTEM : origin = 0x007010, length = 0x000020 /* System control registers */
    SPIA : origin = 0x007040, length = 0x000010 /* SPI-A registers */
    SCIA : origin = 0x007050, length = 0x000010 /* SCI-A registers */
    XINTRUPT : origin = 0x007070, length = 0x000010 /* external interrupt registers */

    ADC : origin = 0x007100, length = 0x000020 /* ADC registers */

    SCIB : origin = 0x007750, length = 0x000010 /* SCI-B registers */

    SCIC : origin = 0x007770, length = 0x000010 /* SCI-C registers */

    I2CA : origin = 0x007900, length = 0x000040 /* I2C-A registers */

    CSM_PWL : origin = 0x33FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations. */

    PARTID : origin = 0x380090, length = 0x000001 /* Part ID register location */
    }


    SECTIONS
    {
    PieVectTableFile : > PIE_VECT, PAGE = 1

    /*** Peripheral Frame 0 Register Structures ***/
    DevEmuRegsFile : > DEV_EMU, PAGE = 1
    FlashRegsFile : > FLASH_REGS, PAGE = 1
    CsmRegsFile : > CSM, PAGE = 1
    AdcMirrorFile : > ADC_MIRROR, PAGE = 1
    XintfRegsFile : > XINTF, PAGE = 1
    CpuTimer0RegsFile : > CPU_TIMER0, PAGE = 1
    CpuTimer1RegsFile : > CPU_TIMER1, PAGE = 1
    CpuTimer2RegsFile : > CPU_TIMER2, PAGE = 1
    PieCtrlRegsFile : > PIE_CTRL, PAGE = 1
    DmaRegsFile : > DMA, PAGE = 1

    /*** Peripheral Frame 3 Register Structures ***/
    McbspaRegsFile : > MCBSPA, PAGE = 1
    McbspbRegsFile : > MCBSPB, PAGE = 1

    /*** Peripheral Frame 1 Register Structures ***/
    ECanaRegsFile : > ECANA, PAGE = 1
    ECanaLAMRegsFile : > ECANA_LAM PAGE = 1
    ECanaMboxesFile : > ECANA_MBOX PAGE = 1
    ECanaMOTSRegsFile : > ECANA_MOTS PAGE = 1
    ECanaMOTORegsFile : > ECANA_MOTO PAGE = 1

    ECanbRegsFile : > ECANB, PAGE = 1
    ECanbLAMRegsFile : > ECANB_LAM PAGE = 1
    ECanbMboxesFile : > ECANB_MBOX PAGE = 1
    ECanbMOTSRegsFile : > ECANB_MOTS PAGE = 1
    ECanbMOTORegsFile : > ECANB_MOTO PAGE = 1

    EPwm1RegsFile : > EPWM1 PAGE = 1
    EPwm2RegsFile : > EPWM2 PAGE = 1
    EPwm3RegsFile : > EPWM3 PAGE = 1
    EPwm4RegsFile : > EPWM4 PAGE = 1
    EPwm5RegsFile : > EPWM5 PAGE = 1
    EPwm6RegsFile : > EPWM6 PAGE = 1

    ECap1RegsFile : > ECAP1 PAGE = 1
    ECap2RegsFile : > ECAP2 PAGE = 1
    ECap3RegsFile : > ECAP3 PAGE = 1
    ECap4RegsFile : > ECAP4 PAGE = 1
    ECap5RegsFile : > ECAP5 PAGE = 1
    ECap6RegsFile : > ECAP6 PAGE = 1

    EQep1RegsFile : > EQEP1 PAGE = 1
    EQep2RegsFile : > EQEP2 PAGE = 1

    GpioCtrlRegsFile : > GPIOCTRL PAGE = 1
    GpioDataRegsFile : > GPIODAT PAGE = 1
    GpioIntRegsFile : > GPIOINT PAGE = 1

    /*** Peripheral Frame 2 Register Structures ***/
    SysCtrlRegsFile : > SYSTEM, PAGE = 1
    SpiaRegsFile : > SPIA, PAGE = 1
    SciaRegsFile : > SCIA, PAGE = 1
    XIntruptRegsFile : > XINTRUPT, PAGE = 1
    AdcRegsFile : > ADC, PAGE = 1
    ScibRegsFile : > SCIB, PAGE = 1
    ScicRegsFile : > SCIC, PAGE = 1
    I2caRegsFile : > I2CA, PAGE = 1

    /*** Code Security Module Register Structures ***/
    CsmPwlFile : > CSM_PWL, PAGE = 1

    /*** Device Part ID Register Structures ***/
    PartIdRegsFile : > PARTID, PAGE = 1

    }


    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
  • In reply to marcello ioppolo1:

    Dear Marcello,
    We will need some additional information please. How is the linker command file that you sent first differ from what you send previously?
    What is the difference between the setup of the section that produces the error and the one that does not. For example, what is the difference between how section GpioDataRegsFile (no error) is setup versus how GpioIntRegsFile (has error).
    Thanks,
    Krishna
  • In reply to Krishna Allam:

    hello, following my answer:
    1) How is the linker command file that you sent first differ from what you send previously?
    im sorry for the mistake the correct linker file is the second one.
    2) For example, what is the difference between how section GpioDataRegsFile (no error) is setup versus how GpioIntRegsFile (has error)?
    we did not modify the standard configuration that can be found in the software downloadable from the control suite for f28335. i report the details for the 2 sections here:

    #ifdef __cplusplus
    #pragma DATA_SECTION("GpioDataRegsFile")
    #else
    #pragma DATA_SECTION(GpioDataRegs,"GpioDataRegsFile");
    #endif

    volatile struct GPIO_DATA_REGS GpioDataRegs;
    struct GPIO_DATA_REGS {
    union GPADAT_REG GPADAT; // GPIO Data Register (GPIO0 to 31)
    union GPADAT_REG GPASET; // GPIO Data Set Register (GPIO0 to 31)
    union GPADAT_REG GPACLEAR; // GPIO Data Clear Register (GPIO0 to 31)
    union GPADAT_REG GPATOGGLE; // GPIO Data Toggle Register (GPIO0 to 31)
    union GPBDAT_REG GPBDAT; // GPIO Data Register (GPIO32 to 63)
    union GPBDAT_REG GPBSET; // GPIO Data Set Register (GPIO32 to 63)
    union GPBDAT_REG GPBCLEAR; // GPIO Data Clear Register (GPIO32 to 63)
    union GPBDAT_REG GPBTOGGLE; // GPIO Data Toggle Register (GPIO32 to 63)
    union GPCDAT_REG GPCDAT; // GPIO Data Register (GPIO64 to 95)
    union GPCDAT_REG GPCSET; // GPIO Data Set Register (GPIO64 to 95)
    union GPCDAT_REG GPCCLEAR; // GPIO Data Clear Register (GPIO64 to 95)
    union GPCDAT_REG GPCTOGGLE; // GPIO Data Toggle Register (GPIO64 to 95)
    Uint16 rsvd1[8];
    };

    #ifdef __cplusplus
    #pragma DATA_SECTION("GpioIntRegsFile")
    #else
    #pragma DATA_SECTION(GpioIntRegs,"GpioIntRegsFile");
    #endif
    volatile struct GPIO_INT_REGS GpioIntRegs;

    struct GPIO_INT_REGS {
    union GPIOXINT_REG GPIOXINT1SEL; // XINT1 GPIO Input Selection
    union GPIOXINT_REG GPIOXINT2SEL; // XINT2 GPIO Input Selection
    union GPIOXINT_REG GPIOXNMISEL; // XNMI_Xint13 GPIO Input Selection
    union GPIOXINT_REG GPIOXINT3SEL; // XINT3 GPIO Input Selection
    union GPIOXINT_REG GPIOXINT4SEL; // XINT4 GPIO Input Selection
    union GPIOXINT_REG GPIOXINT5SEL; // XINT5 GPIO Input Selection
    union GPIOXINT_REG GPIOXINT6SEL; // XINT6 GPIO Input Selection
    union GPIOXINT_REG GPIOXINT7SEL; // XINT7 GPIO Input Selection
    union GPADAT_REG GPIOLPMSEL; // Low power modes GP I/O input select
    };

    bets regards
    marcello
  • In reply to marcello ioppolo1:

    Hi Marcello, Have you been able to resolve the issue that you were seeing?  Thanks for letting me know.   Cheers! Krishna

  • In reply to Krishna Allam:

    hello,

    i found out that my bootloader cannot follow the initial design. In my intention the section 234 and 567 should have stored two relocatables software images but c28x architecture does not allow relocation of the code. i am now using the entire flash memory to store a unique software image which i compile in a standard way.

    best regards.

    marcello ioppolo

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.