error while connecting to ccs idelink error

hello,                                  

  i m having a problem in running TIC2000 demo C2812adcpwmtest using Matlab R2007a ,

its giving error:

Error building Real-Time Workshop target for block diagram 'c2812adcpwmtest'. MATLAB error message:
Error using ==> callMakeHook.p>callMakeHook at 47
The call to ccslink_ert_make_rtw_hook, during the entry hook generated the following error:
    Error using ==> i_entryHookpoint at 52
Error while creating the link for IDE.

The build process will terminate as a result.

while incremental build model using simulink this error window opens ,its not connecting to ccs

Matlab R2007a

TiC2000

F2812  CCS v3.1

dsp kit F2812

demo : C2812adcpwmtest

 

plz help me i m stucked with my project ..............................

5 Replies

  • deepika shukla

    hello,                                  

      i m having a problem in running TIC2000 demo C2812adcpwmtest using Matlab R2007a ,

    its giving error:

    Error building Real-Time Workshop target for block diagram 'c2812adcpwmtest'. MATLAB error message:
    Error using ==> callMakeHook.p>callMakeHook at 47
    The call to ccslink_ert_make_rtw_hook, during the entry hook generated the following error:
        Error using ==> i_entryHookpoint at 52
    Error while creating the link for IDE.

    The build process will terminate as a result.

    while incremental build model using simulink this error window opens ,its not connecting to ccs

    Matlab R2007a

    TiC2000

    F2812  CCS v3.1

    dsp kit F2812

    demo : C2812adcpwmtest

     

    plz help me i m stucked with my project ..............................

    Unfortunately I do not have an answer to offer you.  I suggest you send the question to c2000_expert@mathworks.com for their advice. 

    Thank you & Regards

    Lori

     

    Did a reply answer your question? If yes, please click the "yes" button located at the bottom of that post.
    Visit these helpful C2000 Links!
    C2000 TI Wiki Pages
    TI Forum Sitemap
    ControlSUITE
    C2000 Getting Started
    CLA FAQs
    Workshop Material!
  • I am getting the following error while building my simulink model to generate the C code.

     

    Error building Real-Time Workshop target for block diagram 'dspafxr'. MATLAB error message:

    Error using ==> callMakeHook.p>callMakeHook at 47

    The call to ccslink_ert_make_rtw_hook, during the entry hook generated the following error:

        Error using ==> i_entryHookpoint at 52

    Error while creating the link for IDE.a                                                                                                    

     

    The build process will terminate as a result.

     

    I am using

    Matlab R2007A

    CCS v3.1

    c6713dsk

     

    can u please help me ? I need it for my project badly...

    plz help me...

  • In reply to Sujeet Kumar Padhi:

    hi sujeet,

    could u tell me the procedure, you r using to to connect to processor.......
    may be then i could help u....

    bye
  • In reply to deepika shukla:

    hiii deepika,

    The procedure is given below:

    We are trying to load the  "audio reverberation" in the board.  (dspafxr.mdl)

    we are connecting the "discrete sine" block at the input and "time scope" at the output.

    1) "custom board" is dragged into the model.

    2) Double click on the board, then the following settings are done

        board info:

            board type: custom

           Processor: 6713

           simulator is chosen.

           operating system : none

           board name : C6713 Device cycle accurate simulator

           Processor name : TMS320C6713

    Memory :

          Only IRAM is chosen.

    section: 

    No change.

    NO change in simulation --> configuration parameters

    can u tell me where is the problem ???

  • In reply to Sujeet Kumar Padhi:

    Hi everyone,

    Somebody resolved this?

    As I have this same problem, I can't complete to build.

    (Error while creating the link for IDE)

    Please tell me the solution.

    My environment is following:

         Matlab R2007a

         CCS v2.21 (I have CCS v3.3 & v5.2.1. But I do not install them.)

         DSP C6713
     

    Rgrds,

         Kaz