hello,
i m having a problem in running TIC2000 demo C2812adcpwmtest using Matlab R2007a ,
its giving error:
Error building Real-Time Workshop target for block diagram 'c2812adcpwmtest'. MATLAB error message:Error using ==> callMakeHook.p>callMakeHook at 47The call to ccslink_ert_make_rtw_hook, during the entry hook generated the following error: Error using ==> i_entryHookpoint at 52Error while creating the link for IDE.The build process will terminate as a result.
while incremental build model using simulink this error window opens ,its not connecting to ccs
Matlab R2007a
TiC2000
F2812 CCS v3.1
dsp kit F2812
demo : C2812adcpwmtest
plz help me i m stucked with my project ..............................
deepika shukla hello, i m having a problem in running TIC2000 demo C2812adcpwmtest using Matlab R2007a , its giving error: Error building Real-Time Workshop target for block diagram 'c2812adcpwmtest'. MATLAB error message:Error using ==> callMakeHook.p>callMakeHook at 47The call to ccslink_ert_make_rtw_hook, during the entry hook generated the following error: Error using ==> i_entryHookpoint at 52Error while creating the link for IDE.The build process will terminate as a result. while incremental build model using simulink this error window opens ,its not connecting to ccs Matlab R2007a TiC2000 F2812 CCS v3.1 dsp kit F2812 demo : C2812adcpwmtest plz help me i m stucked with my project ..............................
Unfortunately I do not have an answer to offer you. I suggest you send the question to c2000_expert@mathworks.com for their advice.
Thank you & Regards
Lori
I am getting the following error while building my simulink model to generate the C code.
Error building Real-Time Workshop target for block diagram 'dspafxr'. MATLAB error message:
Error using ==> callMakeHook.p>callMakeHook at 47
The call to ccslink_ert_make_rtw_hook, during the entry hook generated the following error:
Error using ==> i_entryHookpoint at 52
Error while creating the link for IDE.a
The build process will terminate as a result.
I am using
Matlab R2007A
CCS v3.1
c6713dsk
can u please help me ? I need it for my project badly...
plz help me...
hi sujeet, could u tell me the procedure, you r using to to connect to processor.......may be then i could help u....bye
hiii deepika,
The procedure is given below:
We are trying to load the "audio reverberation" in the board. (dspafxr.mdl)
we are connecting the "discrete sine" block at the input and "time scope" at the output.
1) "custom board" is dragged into the model.
2) Double click on the board, then the following settings are done
board info:
board type: custom
Processor: 6713
simulator is chosen.
operating system : none
board name : C6713 Device cycle accurate simulator
Processor name : TMS320C6713
Memory :
Only IRAM is chosen.
section:
No change.
NO change in simulation --> configuration parameters
can u tell me where is the problem ???
Hi everyone,
Somebody resolved this?
As I have this same problem, I can't complete to build.
(Error while creating the link for IDE)
Please tell me the solution.
My environment is following:
CCS v2.21 (I have CCS v3.3 & v5.2.1. But I do not install them.)
DSP C6713
Rgrds,
Kaz