Greetings,
I have a 3A lower motor current threshold limit on the motor phase, which means i cannot regulate the current <3A. I use sensored control with hall sensors on the DRV8301-HC-C2-KIT. Is there a away to remove this current offset of 3A, so it will be possible to regulate the motor phase current under this 3A limit? If so is it a software or hardware issue and how could i remove it? When i worked with the DRV8312 kit it was possible to regulate the current below 3A and almost up to 0A.
Yours sincerly,
Pavel Ruban