Hi all,
During my study work with the
Concerto-Processor(F28M35H52C1) , my project becomes too big for the RAM memory.
That's why I wanted to load the program in the flash memory, but it didn't work.
So I decided to study the sample project flash_m3 and tried to load this on the
Concerto, but without success.
Error message:
-
Cortex_M3_0: Loader: One or more sections of your program falls into a memory
region that is not writable. These regions will not actually be written to the
target. Check your linker configuration and/or memory map.
-
Cortex_M3_0: File Loader: Data verification failed at address 0x00201000 Please
verify target memory and memory map.
- Cortex_M3_0: Warning:
(Error -1003 @ 0x2BC5) Internal error: Invalid parameter passed to function.
Restart the application. If error persists, please report the error. (Release
5.0.333.0)
- Error found during data
verification.
- Ensure the linker command file matches the memory
map.
I'm using the Code Composer Studio v4 and controlSUITE
v2.5.0.
Can you help me to run the sample project. How can I solve this
problem?
Thank you
Regards
Michael