Hi,
I am working on the HVMotorCtrl+Pfc Kit supplied by TI with C2000 TMS320F28035 micro-controller (control card).
I have succesfully run the code provided into the control suit for this application from the RAM memory.
But when i am configuring it for FLASH memory, following messages are coming while debugging active project. Where to do the changes to get it run from the flash? What changes or settings I have to do?
C28xx: Flash Programmer: Missing Flash Programming Settings.
C28xx: Flash Programmer: Error erasing Flash memory.
C28xx: Flash Programmer: Missing Flash operation option. Operation cancelled.
C28xx: Trouble Writing Memory Block at 0x3f6a44 on Page 0 of Length 0x1d0
Cannot write to target
Regards,
Rupesh