Hi,
IDE: CCSv4
Emulator: SPI515PP
Target: TMS320F2812
I've faced problems while I tried to communicate with SPI515PP through a PCI-Parallel Port Card but it works fine if the PC has a built-in parallel port. The latest PCs do not come with a parallel port.
Does the SPI515PP emulator work properly if the connectivity is through an external PCI-Parallel Port Card?
-Regards
-Sinoj