HI,
I'm using LM FLASH PROGRAMMER build 1429 to do the serial download of my blinky_m3.bin to the M3, with the "reset MCU After Program" checked, and download address of 0x20005000. The programmer reports "Program Complete 21944 Bytes Programmed" but the blinky application doesn't start running. I prepared the .bin file by following the steps for post build in TRM 6.8.1.1 for the blinky_m3 example.
"${CCE_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin.bat" "${BuildArtifactFileName}"
"${BuildArtifactFileBaseName}.bin" "${CG_TOOL_ROOT}/bin/ofd470.exe"
"${CG_TOOL_ROOT}/bin/hex470.exe" "${CCE_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin.exe"
I'm using 64 bit windows 7, and I didn't see the reset, I also tried running it in XP compatibility mode, and didn't see the reset. Any ideas for me?
Thanks,
Larry