Hi,
What is the value of the pull up and pull down resistors on the F2812? I haven't found any information on the documentation... and can they be disabled via SW?
Thanks,
Maite
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Maite,
The internal pullups/downs on F2812 are active circuits, not passive resistors. There is no Ohms rating. Rather, there are current ratings given in the datasheet, SPRS174O, p.93. You can roughly think of these ratings as the amount of current needed to overpower the pullup/down and cause the pin to change logic level.
On F281x devices, the internal pullups/downs cannot be disabled.
Regards,
David