Hi ..
I am working with eCAN module TMS320F28335 experimental kit.
I used ecanA as transmitter and ecanB as receiver and configured mailboxes like in example project of TI.
I am not able to read received massage at eCANB.
6153.eCAN_Tx & Rx.txt
/* CAN Tx and Rx massage main.c */ #include "DSP28x_Project.h" void main(void) { struct ECAN_REGS ECanaShadow; struct ECAN_REGS ECanbShadow; Uint16 temp; InitSysCtrl(); DINT; InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; InitPieVectTable(); EALLOW; GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 1;// Configure GPIO31 for CANTXA operation GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 1;// Configure GPIO30 for CANRXA operation GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 2;// Configure GPIO8 for CANTXB operation GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 2; // Configure GPIO10 for CANRXB operation GpioCtrlRegs.GPBPUD.bit.GPIO34 = 0; GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0; GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1; EDIS; InitECan(); ECanaMboxes.MBOX5.MSGID.all = 0x95555555; ECanaMboxes.MBOX5.MSGID.bit.IDE = 1; ECanbMboxes.MBOX1.MSGID.all = 0x95555555; ECanbMboxes.MBOX1.MSGID.bit.IDE = 1; /* Configure Mailbox 5 as transmit mailbox */ ECanaShadow.CANMD.all = ECanaRegs.CANMD.all; ECanaShadow.CANMD.bit.MD5 = 0; ECanaRegs.CANMD.all = ECanaShadow.CANMD.all; /* Enable Mailbox 5 */ ECanaShadow.CANME.all = ECanaRegs.CANME.all; ECanaShadow.CANME.bit.ME5 = 1; ECanaRegs.CANME.all = ECanaShadow.CANME.all; /* Write to DLC field in Master Control reg */ ECanaMboxes.MBOX5.MSGCTRL.all = 0; ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX5.MDL.all = 0x55555555; ECanaMboxes.MBOX5.MDH.all = 0x55555555; /* Configure Mailbox 1 as Receive mailbox */ ECanbShadow.CANMD.all = ECanbRegs.CANMD.all; ECanbShadow.CANMD.bit.MD1 = 1; ECanbRegs.CANMD.all = ECanbShadow.CANMD.all; /* Enable Mailbox 1 */ ECanbShadow.CANME.all = ECanbRegs.CANME.all; ECanbShadow.CANME.bit.ME1 = 1; ECanbRegs.CANME.all = ECanbShadow.CANME.all; /* Write to DLC field in Master Control reg */ ECanbMboxes.MBOX1.MSGCTRL.all = 0; ECanbMboxes.MBOX1.MSGCTRL.bit.DLC = 8; while(1) { ECanaShadow.CANTRS.all = 0; ECanaShadow.CANTRS.bit.TRS5 = 1; // Set TRS for mailbox under test ECanaRegs.CANTRS.all = ECanaShadow.CANTRS.all; do { ECanaShadow.CANTA.all = ECanaRegs.CANTA.all; } while(ECanaShadow.CANTA.bit.TA5 == 0 );// Wait for TA5 bit to be set. ECanaShadow.CANTA.all = 0; ECanaShadow.CANTA.bit.TA5 = 1; // Clear Transmit Acknowledge #5 ECanaRegs.CANTA.all = ECanaShadow.CANTA.all; if (ECanbRegs.CANRMP.bit.RMP1 == 1) ;// valid new data in MBX1? temp = ECanbMboxes.MBOX1.MDL.byte.BYTE0; // read message ECanbRegs.CANRMP.bit.RMP1 = 1; // clear the status flag RMP1 if(temp & 1) // update LED LD1 GpioDataRegs.GPBSET.bit.GPIO34 = 1; else GpioDataRegs.GPBCLEAR.bit.GPIO34 = 1; // and prepare MBX1 for next receive } }
please find code in attached file.
anyone can correct my code where i am doing mistake.
any suggestion would appreciable.
Thanks
Mehul