hi
suggest me the best solution for , BLDC motor(3-phase,1.1 hp,310v dc,4600rpm,4 poles,5amps) ) with hall sensor in C2000 piccolo or delifino boards along with hardware equipment
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi
suggest me the best solution for , BLDC motor(3-phase,1.1 hp,310v dc,4600rpm,4 poles,5amps) ) with hall sensor in C2000 piccolo or delifino boards along with hardware equipment
Hi,
Why don't you go through this:
http://www.ti.com/lsds/ti/apps/motor/brushless_dc/overview.page
Regards,
Gautam
Hello!
Also please pay attention on these threads
http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/286994.aspx
http://e2e.ti.com/support/applications/motor_drivers/f/38/p/258667/915458.aspx#915458
Regards,
Igor
If you are set on doing hall sensored BLDC you should use TMDSHVMTRPFCKIT, there is a SW example that runs on Piccolo tmdscncd28035. Software support from www.ti.com/tool/controlsuite
I also recommend purchasing TMDSCNCD28069MISO controlCARD which will allow you to plug in to the same Hv inverter and try sensorless InstaSPIN-FOC and sensored or sensorless InstaSPIN-MOTION. These are supported through www.ti.com/tool/motorkitscncd69miso and www.ti.com/tool/motorware
Hi I am a student from Ecuador, I have purchased the TMDSHVMTRPFCKIT, I think it is incredible; recently I have been studying the two control methods for BLDC motor, but I have trouble understanding the HALL3_DRV module used in the Sensored Trapezoidal Control, I wonder if you could explain certain details of the module (operation principle) especially the HALL3_DEBOUNCED_MACRO I have read the software flowcharts on the guide but there is no the technical background.
I have read about the InstaSPIN-FOC technique and I think it is far superior to the other techniques, unfortunately today in my coutry is difficult to import, but as soon as I have the resources I will import it.
documented
C:\ti\controlSUITE\libs\app_libs\motor_control\drivers\f2803x_v2.1\~Docs\DMC2803x_DRV.pdf
you can go read about using hall sensors in general, this may give you a better background than our docs provide on the principle of operation.
Luis Villafuerte said:I have read about the InstaSPIN-FOC technique and I think it is far superior to the other techniques, unfortunately today in my coutry is difficult to import, but as soon as I have the resources I will import it.
Yes, it is! All you need is to purchase
TMDSCNCD28069MISO
and it will work with your TMDSHVMTRPFCKIT if it is Rev 1.1 (yellow PCB